<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: Example MPC5746R FlexCAN</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776249#M11255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the example you use is created in S32 Design Studio v1.1 and unfortunately, it cannot be import and compiled in S32DS 2017.R1, because there were some significant changes in compiler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you create new project in S32DS 2017.R1 and manually copy all necessary source code into new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Dec 2017 09:50:57 GMT</pubDate>
    <dc:creator>martin_kovar</dc:creator>
    <dc:date>2017-12-11T09:50:57Z</dc:date>
    <item>
      <title>Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776248#M11254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having issue getting the CAN Example for the&amp;nbsp;MPC5746R to work?&amp;nbsp; I am using the 57XX mother board with the MPC5746R-252DS.&amp;nbsp; I would expect that this example would just work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified that the pin jumpers J37 and J38 are in the 2-3 position.&amp;nbsp; &amp;nbsp;I have also tried with them in the 1-2 position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using s32DS 2017.R1 and an iSystems debugger.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Dec 2017 20:35:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776248#M11254</guid>
      <dc:creator>ronlewis</dc:creator>
      <dc:date>2017-12-08T20:35:33Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776249#M11255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ron,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the example you use is created in S32 Design Studio v1.1 and unfortunately, it cannot be import and compiled in S32DS 2017.R1, because there were some significant changes in compiler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend you create new project in S32DS 2017.R1 and manually copy all necessary source code into new project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 09:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776249#M11255</guid>
      <dc:creator>martin_kovar</dc:creator>
      <dc:date>2017-12-11T09:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776250#M11256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I did not have any issues compiling the example.&amp;nbsp; Example compiles and runs on the hardware, but I don't see any activity on the CAN bus. I did create a new project in 2017.R1 and copied over the the code from the FlexCAN project, but I still don't see any CAN Activity.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 15:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776250#M11256</guid>
      <dc:creator>ronlewis</dc:creator>
      <dc:date>2017-12-11T15:22:56Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776251#M11257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &amp;nbsp;Ron,&lt;/P&gt;&lt;P&gt;I had tried it and found a problem. CAN2 has 64 MessageBuffer, but it just has 8 MB can be using.&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am very confused.&amp;nbsp;Can you explain it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 06:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776251#M11257</guid>
      <dc:creator>flyskyr丶</dc:creator>
      <dc:date>2018-06-20T06:45:01Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776252#M11258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not sure I understand your question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The example from above uses MB[0] to receive a message on CAN2,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jun 2018 11:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776252#M11258</guid>
      <dc:creator>ronlewis</dc:creator>
      <dc:date>2018-06-20T11:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: Example MPC5746R FlexCAN</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776253#M11259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ron,&lt;/P&gt;&lt;P&gt;I found and&amp;nbsp;solved this problem.&lt;/P&gt;&lt;P&gt;When using your configuration&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62509iF55E2CDE2A989704/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;MAXMB in this register is not set to 0x3F successfully, it is 0xF. Because of that "This field can be&lt;BR /&gt;written only in Freeze mode because it is blocked by hardware in other modes".&amp;nbsp;Only 16 MBs can be used in this case.&lt;/P&gt;&lt;P&gt;So I add that "CAN_1.MCR.B.MAXMB = 63;". Now , 64 MBs can be used. it's fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 01:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Example-MPC5746R-FlexCAN/m-p/776253#M11259</guid>
      <dc:creator>flyskyr丶</dc:creator>
      <dc:date>2018-06-27T01:26:02Z</dc:date>
    </item>
  </channel>
</rss>