<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC5500 Flash Driver Demo Error in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5500-Flash-Driver-Demo-Error/m-p/775799#M11246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried the MPC5500 Flash Driver on the MPC5566 and&amp;nbsp;the Demo&amp;nbsp;works just fine except one little thing.&lt;/P&gt;&lt;P&gt;pChecksum in the demo code returns a sum not equal to 0 as the content of the address range 0x00080000-0x0008001F changes from 0x00000000&amp;nbsp;to 0xFFFFFFFF after the execution of pFlashProgram and pProgramVerify. On first execution of pFlashProgram the data is initialised to 0 as expected but something changes it at the end.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced the write acccess to the address 0x00080000 and this occurs only once&amp;nbsp;during the first execution of pFlashProgram when the&amp;nbsp;content is changed to 0x00000000&amp;nbsp;so the code seems not to set it back to 0xFFFFFFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have an idea what happens there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Dec 2017 15:04:01 GMT</pubDate>
    <dc:creator>michaelwichmann</dc:creator>
    <dc:date>2017-12-08T15:04:01Z</dc:date>
    <item>
      <title>MPC5500 Flash Driver Demo Error</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5500-Flash-Driver-Demo-Error/m-p/775799#M11246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I tried the MPC5500 Flash Driver on the MPC5566 and&amp;nbsp;the Demo&amp;nbsp;works just fine except one little thing.&lt;/P&gt;&lt;P&gt;pChecksum in the demo code returns a sum not equal to 0 as the content of the address range 0x00080000-0x0008001F changes from 0x00000000&amp;nbsp;to 0xFFFFFFFF after the execution of pFlashProgram and pProgramVerify. On first execution of pFlashProgram the data is initialised to 0 as expected but something changes it at the end.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced the write acccess to the address 0x00080000 and this occurs only once&amp;nbsp;during the first execution of pFlashProgram when the&amp;nbsp;content is changed to 0x00000000&amp;nbsp;so the code seems not to set it back to 0xFFFFFFFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have an idea what happens there?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Dec 2017 15:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5500-Flash-Driver-Demo-Error/m-p/775799#M11246</guid>
      <dc:creator>michaelwichmann</dc:creator>
      <dc:date>2017-12-08T15:04:01Z</dc:date>
    </item>
  </channel>
</rss>