<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC5645S Dram driver in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768946#M11026</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;I confirm that the CPU code cannot modify the DRAM even with the DCU not in operation.&lt;/P&gt;&lt;P&gt;There is no problem to modify the DRAM with the debugger. The ram tests that I perform with the debugger are OK.&lt;/P&gt;&lt;P&gt;I would be glad to have some source code that is ready to run on the&amp;nbsp; MPC5645S demo board that exercises the DRAM interface.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2018 10:29:20 GMT</pubDate>
    <dc:creator>deniszallot</dc:creator>
    <dc:date>2018-04-06T10:29:20Z</dc:date>
    <item>
      <title>MPC5645S Dram driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768944#M11024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I work on the MPC5645S evaluation board.&lt;/P&gt;&lt;P&gt;I have written a DRAM driver.&lt;/P&gt;&lt;P&gt;I have noticed that the DCU can access this DRAM because when I modify the content of the DRAM, the TFT changes color.&lt;/P&gt;&lt;P&gt;On the other hand, I cannot have the E200z4 core write in it.&lt;/P&gt;&lt;P&gt;Also, the DRAM tests that I performed with the Green Hill debugger is OK&lt;/P&gt;&lt;P&gt;My ram is mapped at address 0x20000000. I hope that the DRAM at this address can be be accessed by the e200z4&lt;/P&gt;&lt;P&gt;Has anybody got a clue of what may be happening?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2018 11:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768944#M11024</guid>
      <dc:creator>deniszallot</dc:creator>
      <dc:date>2018-04-05T11:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S Dram driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768945#M11025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I understand you well you can modify DRAM content by debugger but not by CPU code as DRAM is occupied by DCU accesses, right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2018 18:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768945#M11025</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-04-05T18:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S Dram driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768946#M11026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;I confirm that the CPU code cannot modify the DRAM even with the DCU not in operation.&lt;/P&gt;&lt;P&gt;There is no problem to modify the DRAM with the debugger. The ram tests that I perform with the debugger are OK.&lt;/P&gt;&lt;P&gt;I would be glad to have some source code that is ready to run on the&amp;nbsp; MPC5645S demo board that exercises the DRAM interface.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 10:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768946#M11026</guid>
      <dc:creator>deniszallot</dc:creator>
      <dc:date>2018-04-06T10:29:20Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5645S Dram driver</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768947#M11027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have working code for DRAM configuration accessed by CPU. Please create new case with link to this MCU and will send it to you. Thanks for understanding:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 08:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5645S-Dram-driver/m-p/768947#M11027</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2018-04-10T08:27:51Z</dc:date>
    </item>
  </channel>
</rss>