<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: How can I use dataflow exception using SPEFSCR?</title>
    <link>https://community.nxp.com/t5/MPC5xxx/How-can-I-use-dataflow-exception-using-SPEFSCR/m-p/759785#M10751</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how did you update the SRR0? There's application note AN4648 which describes how to increment the address in SRR0:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4648.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4648.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Feb 2018 09:36:08 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2018-02-21T09:36:08Z</dc:date>
    <item>
      <title>How can I use dataflow exception using SPEFSCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-can-I-use-dataflow-exception-using-SPEFSCR/m-p/759784#M10750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, dear.&lt;/P&gt;&lt;P&gt;I'm using mpc5773 and have a question about SPEFSCR.&lt;/P&gt;&lt;P&gt;For using under, divide 0, invalid exception, I made some bits to 1. -&amp;gt; set&amp;nbsp;SPEFSCR value : 0x0000 0039&lt;/P&gt;&lt;P&gt;and made Interrupt is&amp;nbsp;occured when an exception is occured.&lt;/P&gt;&lt;P&gt;But, when Interrupt is occured, back to address which stored in&amp;nbsp;SRR0. So,&amp;nbsp;&amp;nbsp;Proceed again the operation that caused the exception. and again and again.&lt;/P&gt;&lt;P&gt;I try to update SRR0 value and it can, but SRR0 value is return to original value after SRR0 update.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;e_lmvsrrw 0x8(r1)&lt;/STRONG&gt; make SRR0 value is return to original value.&lt;/P&gt;&lt;P&gt;as a result, I can't get out of the exception. Could you give me a tip or some help?&lt;/P&gt;&lt;P&gt;(I already make some flags(FINVS, FDBZS, FUNFS) clear when exception occured.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 04:39:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-can-I-use-dataflow-exception-using-SPEFSCR/m-p/759784#M10750</guid>
      <dc:creator>민지혜</dc:creator>
      <dc:date>2018-02-20T04:39:42Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use dataflow exception using SPEFSCR?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/How-can-I-use-dataflow-exception-using-SPEFSCR/m-p/759785#M10751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;how did you update the SRR0? There's application note AN4648 which describes how to increment the address in SRR0:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4648.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN4648.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 09:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/How-can-I-use-dataflow-exception-using-SPEFSCR/m-p/759785#M10751</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2018-02-21T09:36:08Z</dc:date>
    </item>
  </channel>
</rss>