<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックRe: MPC5777M DMAMUX source slot mapping</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752739#M10552</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;see Table 7-26. &lt;EM&gt;DMAMUX peripheral DMA request to input source mapping&lt;/EM&gt; of the device RM;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf" title="https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 04:52:00 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2018-06-06T04:52:00Z</dc:date>
    <item>
      <title>MPC5777M DMAMUX source slot mapping</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752738#M10551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could anybody provide the MPC5777M DMAMUX source slot mapping? This information is missing in the MPC5777M Reference Manual. Where could I find it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In chapter 25.3.1 (from MPC5777M Reference Manual) the Channel Configuration register (DMAMUX_CHCFGn) contains a field called SOURCE specifing which DMA source (slot), if any, is routed to a particular DMA channel. See the chip-specific DMAMUX information for details about the peripherals and their slot numbers. But this information I did not find anywhere.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 13:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752738#M10551</guid>
      <dc:creator>gelumovileanu</dc:creator>
      <dc:date>2018-06-05T13:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M DMAMUX source slot mapping</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752739#M10552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;see Table 7-26. &lt;EM&gt;DMAMUX peripheral DMA request to input source mapping&lt;/EM&gt; of the device RM;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf" title="https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf"&gt;https://www.nxp.com/docs/en/reference-manual/MPC5777MRM.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 04:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752739#M10552</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2018-06-06T04:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5777M DMAMUX source slot mapping</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752740#M10553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you very much, I did not notice it. I looked for “source slot mapping” like for the other processors.&lt;/P&gt;&lt;P&gt;All the best!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Gelu Movileanu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: PetrS &lt;/P&gt;&lt;P&gt;Gesendet: Mittwoch, 6. Juni 2018 06:53&lt;/P&gt;&lt;P&gt;An: Gelu Movileanu &amp;lt;gelu.movileanu@lsp-ias.com&amp;gt;&lt;/P&gt;&lt;P&gt;Betreff: Re:  - Re: MPC5777M DMAMUX source slot mapping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: MPC5777M DMAMUX source slot mapping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Petr Stancik&amp;lt;https://community.nxp.com/people/PetrS?et=watches.email.thread&amp;gt; in MPC5xxx - View the full discussion&amp;lt;https://community.nxp.com/message/1021505?commentID=1021505&amp;amp;et=watches.email.thread#comment-1021505&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 06:12:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5777M-DMAMUX-source-slot-mapping/m-p/752740#M10553</guid>
      <dc:creator>gelumovileanu</dc:creator>
      <dc:date>2018-06-06T06:12:12Z</dc:date>
    </item>
  </channel>
</rss>