<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Hardware bug in erasing? in MPC5xxx</title>
    <link>https://community.nxp.com/t5/MPC5xxx/Hardware-bug-in-erasing/m-p/745939#M10344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MPC5674f when FlashA M1 is erased it erase also H5 and other way execution erasing H5 destroys also M1.&lt;/P&gt;&lt;P&gt;The mask i am using for M1 erase_mask = 0xFFFDFFFF; and for H5 erase_mask = 0xFFFFFFDF;&lt;/P&gt;&lt;P&gt;Could anyone to confirm this? Is it hw bug?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jun 2018 14:13:01 GMT</pubDate>
    <dc:creator>oloooloo</dc:creator>
    <dc:date>2018-06-01T14:13:01Z</dc:date>
    <item>
      <title>Hardware bug in erasing?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Hardware-bug-in-erasing/m-p/745939#M10344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In MPC5674f when FlashA M1 is erased it erase also H5 and other way execution erasing H5 destroys also M1.&lt;/P&gt;&lt;P&gt;The mask i am using for M1 erase_mask = 0xFFFDFFFF; and for H5 erase_mask = 0xFFFFFFDF;&lt;/P&gt;&lt;P&gt;Could anyone to confirm this? Is it hw bug?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 14:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Hardware-bug-in-erasing/m-p/745939#M10344</guid>
      <dc:creator>oloooloo</dc:creator>
      <dc:date>2018-06-01T14:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware bug in erasing?</title>
      <link>https://community.nxp.com/t5/MPC5xxx/Hardware-bug-in-erasing/m-p/745940#M10345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;looks like problem solved, bootloader is stettng valuses in some registers, if i set them back to 0 erasing works fine, those registers are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; *(unsigned int*)0xC3F91684 = 0x0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xFFF48008 = 0x0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xFFF4816D = 0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xC3FF0000 = 0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xC3FF0100 = 0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xC3FF0108 = 0;&lt;BR /&gt;&amp;nbsp; *(unsigned int*)0xC3FF010C = 0;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 21:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/Hardware-bug-in-erasing/m-p/745940#M10345</guid>
      <dc:creator>oloooloo</dc:creator>
      <dc:date>2018-06-01T21:00:04Z</dc:date>
    </item>
  </channel>
</rss>