<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxx中的主题 Re: MPC5644B FLEXCAN module</title>
    <link>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426037#M1008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also faced the same issue in FlexCAN module of MPC5777C controller. It is transmitting only one CAN frame. after that the FlexCAN is put into Freeze Mode. It is happening with Receive also. After receive one frame the FlexCAN module is put into Freeze mode.&lt;/P&gt;&lt;P&gt;Please help anybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gurumurthy K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 14:41:49 GMT</pubDate>
    <dc:creator>gurumurthykola</dc:creator>
    <dc:date>2015-06-24T14:41:49Z</dc:date>
    <item>
      <title>MPC5644B FLEXCAN module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426036#M1007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have MPC5644B and i am using Flexcan 0 on it.The problem i am facing is that after transmitting first frame,Flexcan dosen't transmit any other frame. The CAN module is receiving frames just fine?&lt;/P&gt;&lt;P&gt;Thanks in advance for help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 04:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426036#M1007</guid>
      <dc:creator>muhammadrafique</dc:creator>
      <dc:date>2015-06-24T04:30:32Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644B FLEXCAN module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426037#M1008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also faced the same issue in FlexCAN module of MPC5777C controller. It is transmitting only one CAN frame. after that the FlexCAN is put into Freeze Mode. It is happening with Receive also. After receive one frame the FlexCAN module is put into Freeze mode.&lt;/P&gt;&lt;P&gt;Please help anybody.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gurumurthy K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 14:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426037#M1008</guid>
      <dc:creator>gurumurthykola</dc:creator>
      <dc:date>2015-06-24T14:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644B FLEXCAN module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426038#M1009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm not sure what's wrong when reading this short description but I can provide very simple example that works as expected. It just sends data from CAN0 to CAN1 and everything is working as expected. See please attachment.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 11:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426038#M1009</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2015-07-01T11:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: MPC5644B FLEXCAN module</title>
      <link>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426039#M1010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Eunjo Lee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 08:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/MPC5644B-FLEXCAN-module/m-p/426039#M1010</guid>
      <dc:creator>eunjolee</dc:creator>
      <dc:date>2016-03-10T08:50:53Z</dc:date>
    </item>
  </channel>
</rss>