<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MPC5xxxのトピックBAF - Serial bootloader support</title>
    <link>https://community.nxp.com/t5/MPC5xxx/BAF-Serial-bootloader-support/m-p/732434#M10002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPC5746C&amp;nbsp; BAF - Serial Boot Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use the serial boot mode (BAF) for programming the code to SRAM. I do not want to use JTAG to program a bootloader, because i want to program the bootloader from serial boot for the first time and then&amp;nbsp; use bootloader for application software flashing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing the following problems:&lt;/P&gt;&lt;P&gt;1. I am confused about how to feed the data to BAF. - As per reference manual, it requires a 64bit default key, start address and length along with no_echo and vle bit followed by data. How do i feed all these inputs to MPC5746C ? What tool should i be using ? i tried to use realterm and tera term with no success. The terminal emulators send data in ascii format. If i feed a hex file, the hex data is treated as ascii and being sent out. Will the BAF code re-convert the ascii data back to hex code ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to use RappID tool, but i want to load the code to 0x40000000. The tool doesnt allow to program data at location less than 0x40001000 as it is a tool for flashing appl from bootloader.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest me how to go ahead.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;BlueBale#BAF#Serial Boot#MPC5746C#Serial Programming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 14:05:29 GMT</pubDate>
    <dc:creator>balachandrakuma</dc:creator>
    <dc:date>2018-01-17T14:05:29Z</dc:date>
    <item>
      <title>BAF - Serial bootloader support</title>
      <link>https://community.nxp.com/t5/MPC5xxx/BAF-Serial-bootloader-support/m-p/732434#M10002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPC5746C&amp;nbsp; BAF - Serial Boot Support&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use the serial boot mode (BAF) for programming the code to SRAM. I do not want to use JTAG to program a bootloader, because i want to program the bootloader from serial boot for the first time and then&amp;nbsp; use bootloader for application software flashing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am facing the following problems:&lt;/P&gt;&lt;P&gt;1. I am confused about how to feed the data to BAF. - As per reference manual, it requires a 64bit default key, start address and length along with no_echo and vle bit followed by data. How do i feed all these inputs to MPC5746C ? What tool should i be using ? i tried to use realterm and tera term with no success. The terminal emulators send data in ascii format. If i feed a hex file, the hex data is treated as ascii and being sent out. Will the BAF code re-convert the ascii data back to hex code ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried to use RappID tool, but i want to load the code to 0x40000000. The tool doesnt allow to program data at location less than 0x40001000 as it is a tool for flashing appl from bootloader.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest me how to go ahead.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;BlueBale#BAF#Serial Boot#MPC5746C#Serial Programming&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 14:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MPC5xxx/BAF-Serial-bootloader-support/m-p/732434#M10002</guid>
      <dc:creator>balachandrakuma</dc:creator>
      <dc:date>2018-01-17T14:05:29Z</dc:date>
    </item>
  </channel>
</rss>