<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Motor Control and Smart Energy中的主题 Custom KV11/Motor Control PCB: OpenSDA?</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937903#M324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I have developed a custom PCB based off of the FRDM-MC-LVPMSM which also has a&amp;nbsp;MKV11Z64VFM7 on the PCB.&amp;nbsp; I have already successfully tuned our motor with the FRDM-KV11 and FRDM-MC-LVPSM eval boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is I want to be able to tune the motor using my custom PCB.&amp;nbsp; With that being said if I configure the FRDM-KV11 eval board to provide external programming/debugging to my custom PCB I know I can use the OpenSDA debugger/programmer to program the KV11 on my custom PCB but will I also be able to connect to the FreeMaster Tuning GUI using the FRDM-KV11 as the programmer/debugger to my custom PCB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am not clear on if I need to somehow wire UART pins from my custom PCB into the FRDM-KV11 board to establish the Freemaster connection to my custom PCB or if this is somehow done through the OpenSDA interface that is on the FRDM-KV11?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in the schematic that the following UART0 Pins are connected to the OpenSDA Debugger...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART0_RX = PTB16&lt;/P&gt;&lt;P&gt;UART0_TX = PTB17&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have these Pins mapped out to a header on my Custom PCB and I see that the UART0_RX is mapped to J1.6 on the FRDM-KV11 Eval Board but I am not really seeing any convenient way to map in my UART0_TX/PTB17 into the FRDM-KV11 Eval Board to connect my Custom PCB UART0_TX line to the Open SDA interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lastly can you please provide details as to what specifically to do to the FRDM-KV11 Eval Board to allow it to program an external board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Oct 2019 23:12:03 GMT</pubDate>
    <dc:creator>appioninc</dc:creator>
    <dc:date>2019-10-17T23:12:03Z</dc:date>
    <item>
      <title>Custom KV11/Motor Control PCB: OpenSDA?</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937903#M324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I have developed a custom PCB based off of the FRDM-MC-LVPMSM which also has a&amp;nbsp;MKV11Z64VFM7 on the PCB.&amp;nbsp; I have already successfully tuned our motor with the FRDM-KV11 and FRDM-MC-LVPSM eval boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is I want to be able to tune the motor using my custom PCB.&amp;nbsp; With that being said if I configure the FRDM-KV11 eval board to provide external programming/debugging to my custom PCB I know I can use the OpenSDA debugger/programmer to program the KV11 on my custom PCB but will I also be able to connect to the FreeMaster Tuning GUI using the FRDM-KV11 as the programmer/debugger to my custom PCB?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am not clear on if I need to somehow wire UART pins from my custom PCB into the FRDM-KV11 board to establish the Freemaster connection to my custom PCB or if this is somehow done through the OpenSDA interface that is on the FRDM-KV11?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see in the schematic that the following UART0 Pins are connected to the OpenSDA Debugger...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;UART0_RX = PTB16&lt;/P&gt;&lt;P&gt;UART0_TX = PTB17&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have these Pins mapped out to a header on my Custom PCB and I see that the UART0_RX is mapped to J1.6 on the FRDM-KV11 Eval Board but I am not really seeing any convenient way to map in my UART0_TX/PTB17 into the FRDM-KV11 Eval Board to connect my Custom PCB UART0_TX line to the Open SDA interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lastly can you please provide details as to what specifically to do to the FRDM-KV11 Eval Board to allow it to program an external board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 23:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937903#M324</guid>
      <dc:creator>appioninc</dc:creator>
      <dc:date>2019-10-17T23:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: Custom KV11/Motor Control PCB: OpenSDA?</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937904#M325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI &lt;A _jive_internal="true" data-content-finding="Community" data-userid="307575" data-username="appioninc" href="https://community.nxp.com/people/appioninc"&gt;Frank Roberts&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You can use the FRDM on board debugger and the virtal&amp;nbsp; com port, but it is not recommend in the product phase.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you are design the product, I suggest you use the specific debugger, eg, Segger JLINK. About the COM port, you can use the TTL-USB tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have questions about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 12:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937904#M325</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-10-18T12:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: Custom KV11/Motor Control PCB: OpenSDA?</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937905#M326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You do not need a serial port access on your custom board.&amp;nbsp; You can configure the communication with Freemaster through the debug port&amp;nbsp; or&amp;nbsp;the CAN port if it is available.&amp;nbsp; Please see the&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/FMSTERUG.pdf"&gt;Freemaster User's Guide&lt;/A&gt;&amp;nbsp;section&amp;nbsp;1.2.1 Going Around UART and SCI.&lt;/P&gt;&lt;P&gt;I just tested this on my bench and did a screen shot of the Options dialogue box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following instructions assume a JLink probe. I used a JLink-Lite-FSL to&amp;nbsp;show&amp;nbsp;the concept.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Open the Project-&amp;gt; Options.&amp;nbsp; Select the radial button for Plug-in Module.&amp;nbsp; Choose FreeMASTER Segger/JLink Communication Plug-in&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FM_jlink_comm.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/93846iCB75B1ED21CCC2FC/image-size/large?v=v2&amp;amp;px=999" role="button" title="FM_jlink_comm.png" alt="FM_jlink_comm.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you select the Configure.. Button you can test the connection.&lt;/P&gt;&lt;P&gt;Then you can connect to the running target just like you did with the UART connection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2019 16:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937905#M326</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2019-10-18T16:15:44Z</dc:date>
    </item>
    <item>
      <title>Re: Custom KV11/Motor Control PCB: OpenSDA?</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937906#M327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Philip/Kerry,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks for the help and quick responses.&amp;nbsp; We have access to J-LINK's so that is not a problem.&amp;nbsp; Based on your responses I have wrapped up my PCB design and will submit off for manufacturing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks Again!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Frank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Oct 2019 15:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937906#M327</guid>
      <dc:creator>appioninc</dc:creator>
      <dc:date>2019-10-22T15:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: Custom KV11/Motor Control PCB: OpenSDA?</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937907#M328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You are welcome.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you still have the question, just let us know.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If your question is solved, please help to mark the correct answer, just to close this case, thank you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2019 02:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Custom-KV11-Motor-Control-PCB-OpenSDA/m-p/937907#M328</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-10-24T02:48:52Z</dc:date>
    </item>
  </channel>
</rss>