<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DRM128 source code in Motor Control and Smart Energy</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/DRM128-source-code/m-p/812821#M257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Benjamin,&lt;/P&gt;&lt;P&gt;As you know that there are multiple peripherals which can decode Encoder signal, for example FTM module with quadrature decoder mode, Quadrature Encoder/Decoder module, QuadTimer module...., different processor have different peripherals, what is your part number?&lt;/P&gt;&lt;P&gt;The encoder can output PhaseA/PhaseB even Home and Index signals, the decoder can counts falling/rising edges of PhaseA and PhaseB signals and give position inf and speed inf.&lt;/P&gt;&lt;P&gt;Unfortunately, I have not the source code for PMSM control with Encoder based on Kinetis, but I have the code based on DSC, I attach it, pls refer to it.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Jun 2018 03:36:40 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-06-26T03:36:40Z</dc:date>
    <item>
      <title>DRM128 source code</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/DRM128-source-code/m-p/812820#M256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an application code example which shows how an FTM output can be used to get position and speed?&amp;nbsp; I'm curious what the suggested way to use the various fixed point datatypes is.&amp;nbsp; All the available examples for Kinetis seem to use sensorless control and the source for the&amp;nbsp;RD3PHASEPMSMVCQE reference design is gone.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Said otherwise, I'd like to find the application code corresponding to DRM128.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ben&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Jun 2018 19:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/DRM128-source-code/m-p/812820#M256</guid>
      <dc:creator>bwillis</dc:creator>
      <dc:date>2018-06-24T19:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: DRM128 source code</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/DRM128-source-code/m-p/812821#M257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Benjamin,&lt;/P&gt;&lt;P&gt;As you know that there are multiple peripherals which can decode Encoder signal, for example FTM module with quadrature decoder mode, Quadrature Encoder/Decoder module, QuadTimer module...., different processor have different peripherals, what is your part number?&lt;/P&gt;&lt;P&gt;The encoder can output PhaseA/PhaseB even Home and Index signals, the decoder can counts falling/rising edges of PhaseA and PhaseB signals and give position inf and speed inf.&lt;/P&gt;&lt;P&gt;Unfortunately, I have not the source code for PMSM control with Encoder based on Kinetis, but I have the code based on DSC, I attach it, pls refer to it.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Jun 2018 03:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/DRM128-source-code/m-p/812821#M257</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-06-26T03:36:40Z</dc:date>
    </item>
  </channel>
</rss>