<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Motor Control and Smart Energy中的主题 c</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/c/m-p/805171#M250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing a control for a 4 phase motor with 4 coils fed @ 90 deg phase shift. All the NXP controls I see are 3 phase; however there are many motion control apps that use 4 phase i.e. turn tables, bikes etc. Mine is a PM motor. The chip I use is MC33033 which also actually does 4 phase control AND HAS 4 outputs for the 4 phases. Are there any NXP&amp;nbsp; devices&amp;nbsp;that I can connect&amp;nbsp;to the MC33033 to get 4 phase control? So all I do is connect my 4 motor coils to the NXP devices?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 09 Sep 2018 14:36:26 GMT</pubDate>
    <dc:creator>kendias</dc:creator>
    <dc:date>2018-09-09T14:36:26Z</dc:date>
    <item>
      <title>c</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/c/m-p/805171#M250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing a control for a 4 phase motor with 4 coils fed @ 90 deg phase shift. All the NXP controls I see are 3 phase; however there are many motion control apps that use 4 phase i.e. turn tables, bikes etc. Mine is a PM motor. The chip I use is MC33033 which also actually does 4 phase control AND HAS 4 outputs for the 4 phases. Are there any NXP&amp;nbsp; devices&amp;nbsp;that I can connect&amp;nbsp;to the MC33033 to get 4 phase control? So all I do is connect my 4 motor coils to the NXP devices?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Sep 2018 14:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/c/m-p/805171#M250</guid>
      <dc:creator>kendias</dc:creator>
      <dc:date>2018-09-09T14:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: c</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/c/m-p/805172#M251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, NXP doesn't provide 4 phase PMSM reference design.&lt;/P&gt;&lt;P&gt;Please check available PMSM reference design from NXP with below link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/applications/solutions/internet-of-things/smart-things/motion-and-motor-control/permanent-magnet-synchronous-motor:PMSM-MOTORS" title="https://www.nxp.com/applications/solutions/internet-of-things/smart-things/motion-and-motor-control/permanent-magnet-synchronous-motor:PMSM-MOTORS"&gt;Permanent Magnet Synchronous Motor (PMSM) Solutions|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Sep 2018 06:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/c/m-p/805172#M251</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-09-11T06:19:09Z</dc:date>
    </item>
  </channel>
</rss>