<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis KM34 AFE Hardware Triggering in Motor Control and Smart Energy</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Kinetis-KM34-AFE-Hardware-Triggering/m-p/715101#M168</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Shmuel,&lt;/P&gt;&lt;P&gt;Regarding your question, as you know that the KM34 has crossbar module, which provide the channel to enable the signals to trigger AFE. you can see the "AFE channel0 trigger" on the table, you can route the XBAR inputs triggering source(the left side of the table3-24) to trigger AFE channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pls refer to the following figure:&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4012i9EFA948E561EBE07/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Sep 2017 05:30:35 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-09-28T05:30:35Z</dc:date>
    <item>
      <title>Kinetis KM34 AFE Hardware Triggering</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Kinetis-KM34-AFE-Hardware-Triggering/m-p/715100#M167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where can I find more information&amp;nbsp;on how to use hardware triggering for the&amp;nbsp;Kinetis MKM34Z256VLx7?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual says "The hardware trigger source is device specific" but I can't seem to find this info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 21:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Kinetis-KM34-AFE-Hardware-Triggering/m-p/715100#M167</guid>
      <dc:creator>sbranover</dc:creator>
      <dc:date>2017-09-27T21:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KM34 AFE Hardware Triggering</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Kinetis-KM34-AFE-Hardware-Triggering/m-p/715101#M168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Shmuel,&lt;/P&gt;&lt;P&gt;Regarding your question, as you know that the KM34 has crossbar module, which provide the channel to enable the signals to trigger AFE. you can see the "AFE channel0 trigger" on the table, you can route the XBAR inputs triggering source(the left side of the table3-24) to trigger AFE channel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pls refer to the following figure:&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4012i9EFA948E561EBE07/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2017 05:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Kinetis-KM34-AFE-Hardware-Triggering/m-p/715101#M168</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-09-28T05:30:35Z</dc:date>
    </item>
  </channel>
</rss>