<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KM34 Modulo seems to stop DMA in Motor Control and Smart Energy</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/KM34-Modulo-seems-to-stop-DMA/m-p/696596#M143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out that the modulo is in reference to the address in memory and not to the start address. When using GCC you can&amp;nbsp;can use (complete code attached):&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;__attribute__ ((aligned ()))‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Oct 2017 00:11:49 GMT</pubDate>
    <dc:creator>sbranover</dc:creator>
    <dc:date>2017-10-10T00:11:49Z</dc:date>
    <item>
      <title>KM34 Modulo seems to stop DMA</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/KM34-Modulo-seems-to-stop-DMA/m-p/696595#M142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I enable the modulo setting on the KM34&amp;nbsp;the DMA transfer seems to terminate before the transfer is complete.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To demonstrate, I've attached a slightly modified version of the&amp;nbsp;DMA memory to memory transfer example.The changes from the original example code are that&amp;nbsp;the buffer is longer and the modulo is enabled.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339028"&gt;dma_memory_to_memory.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 17:45:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/KM34-Modulo-seems-to-stop-DMA/m-p/696595#M142</guid>
      <dc:creator>sbranover</dc:creator>
      <dc:date>2017-10-02T17:45:05Z</dc:date>
    </item>
    <item>
      <title>Re: KM34 Modulo seems to stop DMA</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/KM34-Modulo-seems-to-stop-DMA/m-p/696596#M143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out that the modulo is in reference to the address in memory and not to the start address. When using GCC you can&amp;nbsp;can use (complete code attached):&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;__attribute__ ((aligned ()))‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Oct 2017 00:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/KM34-Modulo-seems-to-stop-DMA/m-p/696596#M143</guid>
      <dc:creator>sbranover</dc:creator>
      <dc:date>2017-10-10T00:11:49Z</dc:date>
    </item>
  </channel>
</rss>