<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Motor Control and Smart Energy中的主题 Sensorless PMSM Field-Oriented Control V2</title>
    <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Sensorless-PMSM-Field-Oriented-Control-V2/m-p/2360424#M1373</link>
    <description>&lt;P&gt;I am currently implementing sensorless control for PMSM using field-oriented control in combination with the AMCLIB_PMSMBemfObsrvDQ and the AMCLIB_TrackObsrv for the ARM Cortex M7F. I have a several kW motor with a mechanical speed sensor mounted to the shaft. I am using as a reference the DRM148 Rev.1, 02/2016.&lt;/P&gt;&lt;P&gt;I would like to achieve a situation where I have sensored closed-loop FOC with an observer running in parallel in the background fed with the right feedback information such that in a steady-state condition the measured (sensor) speed and the estimated observer speed converge. Referring back to Fig. 23, from the DRM148, the estimated observer speed is converging near the open-loop speed during start-up.&lt;/P&gt;&lt;P&gt;In the AMCLIB_PMSMBemfObsrvDQ I use the sensor speed output (converted to angular electrical rotor speed) as an input to the BEMF observer from standstill (so no open-loop startup). From 0 - 100 RPM the observer is initialized, whereas for speed &amp;gt;100 RPM it uses feedback and the init function is not used anymore. Furthermore, the requested voltages (Udq*) and currents (Idq*) are used for the BEMF observer input(s). I convert the AMCLIB_TrackObsrv output electrical rotor speed to mechanical speed in RPM and visually compare this to the actual rotor/sensor mechanical shaft speed. This all happens in closed-loop manner (sensored). However, the AMCLIB_TrackObsrv output speed still does not converge on a long time frame (e.g. &amp;gt;10 seconds) while keeping the rotor speed constant (e.g. 500 RPM). This is in no-load condition. When applying load to the motor shaft the estimated mechanical speed from the observer decreases rapidly.&lt;/P&gt;&lt;P&gt;What are possible causes for this difference in RPM between the true sensor mechanical speed and the estimated observer mechanical speed when using sensored closed-loop control?&lt;/P&gt;</description>
    <pubDate>Tue, 05 May 2026 10:39:34 GMT</pubDate>
    <dc:creator>General_motor_control</dc:creator>
    <dc:date>2026-05-05T10:39:34Z</dc:date>
    <item>
      <title>Sensorless PMSM Field-Oriented Control V2</title>
      <link>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Sensorless-PMSM-Field-Oriented-Control-V2/m-p/2360424#M1373</link>
      <description>&lt;P&gt;I am currently implementing sensorless control for PMSM using field-oriented control in combination with the AMCLIB_PMSMBemfObsrvDQ and the AMCLIB_TrackObsrv for the ARM Cortex M7F. I have a several kW motor with a mechanical speed sensor mounted to the shaft. I am using as a reference the DRM148 Rev.1, 02/2016.&lt;/P&gt;&lt;P&gt;I would like to achieve a situation where I have sensored closed-loop FOC with an observer running in parallel in the background fed with the right feedback information such that in a steady-state condition the measured (sensor) speed and the estimated observer speed converge. Referring back to Fig. 23, from the DRM148, the estimated observer speed is converging near the open-loop speed during start-up.&lt;/P&gt;&lt;P&gt;In the AMCLIB_PMSMBemfObsrvDQ I use the sensor speed output (converted to angular electrical rotor speed) as an input to the BEMF observer from standstill (so no open-loop startup). From 0 - 100 RPM the observer is initialized, whereas for speed &amp;gt;100 RPM it uses feedback and the init function is not used anymore. Furthermore, the requested voltages (Udq*) and currents (Idq*) are used for the BEMF observer input(s). I convert the AMCLIB_TrackObsrv output electrical rotor speed to mechanical speed in RPM and visually compare this to the actual rotor/sensor mechanical shaft speed. This all happens in closed-loop manner (sensored). However, the AMCLIB_TrackObsrv output speed still does not converge on a long time frame (e.g. &amp;gt;10 seconds) while keeping the rotor speed constant (e.g. 500 RPM). This is in no-load condition. When applying load to the motor shaft the estimated mechanical speed from the observer decreases rapidly.&lt;/P&gt;&lt;P&gt;What are possible causes for this difference in RPM between the true sensor mechanical speed and the estimated observer mechanical speed when using sensored closed-loop control?&lt;/P&gt;</description>
      <pubDate>Tue, 05 May 2026 10:39:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/Sensorless-PMSM-Field-Oriented-Control-V2/m-p/2360424#M1373</guid>
      <dc:creator>General_motor_control</dc:creator>
      <dc:date>2026-05-05T10:39:34Z</dc:date>
    </item>
  </channel>
</rss>