<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with MCUXpresso for VSCode SWO Console output in MCUXpresso for VSCode</title>
    <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Problem-with-MCUXpresso-for-VSCode-SWO-Console-output/m-p/2392398#M579</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setup&lt;/STRONG&gt;&lt;BR /&gt;MCUXpresso for VSCode&lt;BR /&gt;Board KW47-LOC&lt;BR /&gt;Project kw47loc_hello_world_swo_cm33_core0&lt;BR /&gt;LinkServer 25.6.131 or 26.3.123&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Description&lt;/STRONG&gt;&lt;BR /&gt;I want to test the SWO capabilities so it can be used with my custom board. On MCUXpresso IDE, it's working well, but on MCUXpresso for VSCode, I have the issue where the SWO console will stop displaying serial output after ~30s. This is really constant.&lt;/P&gt;&lt;P&gt;Steps to reproduce&lt;BR /&gt;- Start a debugging session with the board and project&lt;BR /&gt;- Halt on main, then press continue&lt;BR /&gt;- Pause the execution, then configure SWO clock via the Analysis window&lt;BR /&gt;- Run SWO ITM via the Probe window&lt;BR /&gt;- Select MCUXpresso SWO console via Output, then resume the execution&lt;BR /&gt;- Serial output start displaying, then after ~30s it hangs&lt;/P&gt;&lt;P&gt;Thank you for your time!&lt;/P&gt;</description>
    <pubDate>Wed, 08 Jul 2026 13:43:40 GMT</pubDate>
    <dc:creator>ilachance-oti</dc:creator>
    <dc:date>2026-07-08T13:43:40Z</dc:date>
    <item>
      <title>Problem with MCUXpresso for VSCode SWO Console output</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Problem-with-MCUXpresso-for-VSCode-SWO-Console-output/m-p/2392398#M579</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Setup&lt;/STRONG&gt;&lt;BR /&gt;MCUXpresso for VSCode&lt;BR /&gt;Board KW47-LOC&lt;BR /&gt;Project kw47loc_hello_world_swo_cm33_core0&lt;BR /&gt;LinkServer 25.6.131 or 26.3.123&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Description&lt;/STRONG&gt;&lt;BR /&gt;I want to test the SWO capabilities so it can be used with my custom board. On MCUXpresso IDE, it's working well, but on MCUXpresso for VSCode, I have the issue where the SWO console will stop displaying serial output after ~30s. This is really constant.&lt;/P&gt;&lt;P&gt;Steps to reproduce&lt;BR /&gt;- Start a debugging session with the board and project&lt;BR /&gt;- Halt on main, then press continue&lt;BR /&gt;- Pause the execution, then configure SWO clock via the Analysis window&lt;BR /&gt;- Run SWO ITM via the Probe window&lt;BR /&gt;- Select MCUXpresso SWO console via Output, then resume the execution&lt;BR /&gt;- Serial output start displaying, then after ~30s it hangs&lt;/P&gt;&lt;P&gt;Thank you for your time!&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jul 2026 13:43:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Problem-with-MCUXpresso-for-VSCode-SWO-Console-output/m-p/2392398#M579</guid>
      <dc:creator>ilachance-oti</dc:creator>
      <dc:date>2026-07-08T13:43:40Z</dc:date>
    </item>
  </channel>
</rss>