<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso for VSCodeのトピックRe: Error 103: Linkserver GDB server quit unexpectedly</title>
    <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377904#M553</link>
    <description>&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;Thanks for that, I am using import from repository and you only get boards to select. Which json does linkserver pull that from? I am supposing I can keep the board and modify the launch config? Otherwise, picking the frdm-MCXW72 as the board does not show the examples that I am trying to import and run.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;</description>
    <pubDate>Sat, 06 Jun 2026 18:07:37 GMT</pubDate>
    <dc:creator>brianmohlman</dc:creator>
    <dc:date>2026-06-06T18:07:37Z</dc:date>
    <item>
      <title>Error 103: Linkserver GDB server quit unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377901#M551</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am starting to develop with the FRDM-MCXW72-LOC boards and I can import, compile examples successfully, when I try to debug linkserver quits with the following in the terminal window:&lt;/P&gt;&lt;P&gt;Waiting for GDB server to start...&lt;BR /&gt;[2026-06-06T13:59:32.968Z] SERVER CONSOLE DEBUG: GDB server connection established. Switch to "DEBUG CONSOLE" to see GDB traces.&lt;BR /&gt;"C:\\NXP\\LinkServer_25.12.83\\LinkServer.exe" -l5 gdbserver "MCXW727CxxxA:MCXW72-LOC" --probe LYHBJEE1C30QX --gdb-port 2336 --no-boot --core cm33_core0 --redlink-port 2440&lt;BR /&gt;[474]DEBUG:asyncio: Using proactor: IocpProactor&lt;BR /&gt;[478]DEBUG:launcher.core.device: Reading devices from JSON files&lt;BR /&gt;[743]DEBUG:launcher.core.device: Finished reading device JSON files&lt;BR /&gt;[747]CRITICAL:__main__: Critical error&lt;BR /&gt;Traceback (most recent call last):&lt;BR /&gt;File "__main__.py", line 44, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "click\core.py", line 1130, in __call__&lt;BR /&gt;File "click\core.py", line 1055, in main&lt;BR /&gt;File "click\core.py", line 1657, in invoke&lt;BR /&gt;File "click\core.py", line 1404, in invoke&lt;BR /&gt;File "click\core.py", line 760, in invoke&lt;BR /&gt;File "launcher\cli\utils\funcs.py", line 152, in wrapper&lt;BR /&gt;File "asyncio\runners.py", line 195, in run&lt;BR /&gt;File "asyncio\runners.py", line 118, in run&lt;BR /&gt;File "asyncio\base_events.py", line 719, in run_until_complete&lt;BR /&gt;File "launcher\cli\cmd\gdbserver.py", line 59, in cmd_gdbserver&lt;BR /&gt;File "contextlib.py", line 214, in __aenter__&lt;BR /&gt;File "launcher\cli\utils\click.py", line 313, in connect&lt;BR /&gt;File "launcher\cli\utils\funcs.py", line 257, in select_device&lt;BR /&gt;File "launcher\cli\utils\funcs.py", line 140, in assert_one_device&lt;BR /&gt;File "launcher\cli\utils\funcs.py", line 129, in die&lt;BR /&gt;Exception: No matching devices&lt;BR /&gt;[2026-06-06T13:59:34.210Z] SERVER CONSOLE DEBUG: GDB server connection closed.&lt;BR /&gt;GDB server connection closed. Terminal will be reused, waiting for next session to start...&lt;/P&gt;&lt;P&gt;I can connect with the linkserver flash app connect to the MCU and flash code. Any ideas why it is not working within MCUXpresso for VSCode environment?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jun 2026 14:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377901#M551</guid>
      <dc:creator>brianmohlman</dc:creator>
      <dc:date>2026-06-06T14:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: Error 103: Linkserver GDB server quit unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377903#M552</link>
      <description>&lt;P&gt;I see there is this error message:&lt;/P&gt;&lt;P&gt;Exception: No matching devices&lt;/P&gt;&lt;P&gt;You have the following device specified:&lt;/P&gt;&lt;P&gt;"MCXW727CxxxA:MCXW72-LOC"&lt;/P&gt;&lt;P&gt;which does not exist at least in my latest version of LinkServer:&lt;/P&gt;&lt;P&gt;C:\NXP\LinkServer_26.5.59&amp;gt;.\LinkServer.exe devices --filter MCXW727CxxxA&lt;BR /&gt;INFO: Exact match for MCXW727CxxxA found&lt;BR /&gt;Family Device Board Cores&lt;BR /&gt;-------- -------- ------- ------------------------&lt;BR /&gt;MCXW7XX MCXW727C cm33_core0, [cm33_core1]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suggest you remove the&amp;nbsp;:MCXW72-LOC for the device selection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jun 2026 16:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377903#M552</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2026-06-06T16:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: Error 103: Linkserver GDB server quit unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377904#M553</link>
      <description>&lt;P&gt;Erich,&lt;/P&gt;&lt;P&gt;Thanks for that, I am using import from repository and you only get boards to select. Which json does linkserver pull that from? I am supposing I can keep the board and modify the launch config? Otherwise, picking the frdm-MCXW72 as the board does not show the examples that I am trying to import and run.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jun 2026 18:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377904#M553</guid>
      <dc:creator>brianmohlman</dc:creator>
      <dc:date>2026-06-06T18:07:37Z</dc:date>
    </item>
    <item>
      <title>Re: Error 103: Linkserver GDB server quit unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377905#M554</link>
      <description>&lt;P&gt;Linkserver has a JSON for MCX-W72-LOC which does not match with the name of the board which is MCXW72-LOC when picking as the board to import examples for. I am attempting copying the original and fixing the naming...Tried and that didn't work, I suppose that there is an issue with linkserver and the MCXW72-LOC board?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jun 2026 18:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Error-103-Linkserver-GDB-server-quit-unexpectedly/m-p/2377905#M554</guid>
      <dc:creator>brianmohlman</dc:creator>
      <dc:date>2026-06-06T18:47:30Z</dc:date>
    </item>
  </channel>
</rss>