<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: rw612 - NXP based modules (ublox) - boards not listed in MCUXpresso for VSCode</title>
    <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188387#M467</link>
    <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/145867"&gt;@DragosMiloiu&lt;/a&gt;&amp;nbsp;worked perfectly. Curious if there is the same setting when building with mcuxpresso sdk and not zephyr?, I want to run some samples from mcuxpresso sdk (freertos based) on the ublox based board &lt;LI-EMOJI id="lia_thinking-face" title=":thinking_face:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Oct 2025 14:53:13 GMT</pubDate>
    <dc:creator>adrianburns1</dc:creator>
    <dc:date>2025-10-17T14:53:13Z</dc:date>
    <item>
      <title>rw612 - NXP based modules (ublox) - boards not listed</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188235#M465</link>
      <description>&lt;P&gt;Hi, im building code for rw612 using a ublox EVK (module IRIS-W1) and would like to use VS Code.&amp;nbsp;&lt;SPAN&gt;When i "Import Example from Repository" then i can only see the NXP boards (attached), not the ublox boards. The version of zephyr supports the ublox board (v4.2.1) and it can be done on command line like this "west build -p always -b ubx_evk_iris_w1 samples/net/dhcpv4_client/" but i would prefer to use VS Code. thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 10:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188235#M465</guid>
      <dc:creator>adrianburns1</dc:creator>
      <dc:date>2025-10-17T10:20:46Z</dc:date>
    </item>
    <item>
      <title>Re: rw612 - NXP based modules (ublox) - boards not listed</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188269#M466</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/255725"&gt;@adrianburns1&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please enable the "Boards Display" option from settings. This will display all boards, not just the ones from NXP folder.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DragosMiloiu_0-1760699744852.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/361390iC7E6F458403F43CC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="DragosMiloiu_0-1760699744852.png" alt="DragosMiloiu_0-1760699744852.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Dragos.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 11:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188269#M466</guid>
      <dc:creator>DragosMiloiu</dc:creator>
      <dc:date>2025-10-17T11:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: rw612 - NXP based modules (ublox) - boards not listed</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188387#M467</link>
      <description>&lt;P&gt;Thanks &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/145867"&gt;@DragosMiloiu&lt;/a&gt;&amp;nbsp;worked perfectly. Curious if there is the same setting when building with mcuxpresso sdk and not zephyr?, I want to run some samples from mcuxpresso sdk (freertos based) on the ublox based board &lt;LI-EMOJI id="lia_thinking-face" title=":thinking_face:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Oct 2025 14:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/rw612-NXP-based-modules-ublox-boards-not-listed/m-p/2188387#M467</guid>
      <dc:creator>adrianburns1</dc:creator>
      <dc:date>2025-10-17T14:53:13Z</dc:date>
    </item>
  </channel>
</rss>