<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using the Link Application to RAM feature in MCUXpresso for VSCode in MCUXpresso for VSCode</title>
    <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Using-the-Link-Application-to-RAM-feature-in-MCUXpresso-for/m-p/2166990#M463</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254481"&gt;@AndrewChoi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please take a look at the following discussion, where my colleague Derek Snell details the process, he did to run an application from RAM on the RT1024. &lt;A href="https://github.com/zephyrproject-rtos/zephyr/discussions/36800" target="_blank"&gt;Run entire application from RAM · zephyrproject-rtos/zephyr · Discussion #36800 · GitHub&lt;/A&gt;. Altough a different device, it is still applicable for the RT1170.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Fri, 12 Sep 2025 21:03:49 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2025-09-12T21:03:49Z</dc:date>
    <item>
      <title>Using the Link Application to RAM feature in MCUXpresso for VSCode</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Using-the-Link-Application-to-RAM-feature-in-MCUXpresso-for/m-p/2164283#M462</link>
      <description>&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;I am developing a system using Zephyr OS on i.MXRT1072&lt;/P&gt;&lt;P&gt;In MCUXpresso IDE, I can use the "Link application to RAM" function to load the binary directly into RAM for testing without programming it in flash. I want to know how to do this in MCUXpresso for VSCode.&lt;/P&gt;&lt;P&gt;After researching the documentation, I found that using the "Link application to RAM" feature in MCUXpresso for VS Code requires directly specifying a memory area to the project's build system. However, trying various methods takes a lot of time and doesn't make any progress.&lt;/P&gt;&lt;P&gt;I think NXP headquarters is also developing Zephyr-related projects by downloading them to RAM. Could you provide an example of how to run the "hello_world" sample in NXP Zephyr V4.1 using NXP Link2 in RAM?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Fri, 05 Sep 2025 09:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Using-the-Link-Application-to-RAM-feature-in-MCUXpresso-for/m-p/2164283#M462</guid>
      <dc:creator>AndrewChoi</dc:creator>
      <dc:date>2025-09-05T09:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: Using the Link Application to RAM feature in MCUXpresso for VSCode</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Using-the-Link-Application-to-RAM-feature-in-MCUXpresso-for/m-p/2166990#M463</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254481"&gt;@AndrewChoi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please take a look at the following discussion, where my colleague Derek Snell details the process, he did to run an application from RAM on the RT1024. &lt;A href="https://github.com/zephyrproject-rtos/zephyr/discussions/36800" target="_blank"&gt;Run entire application from RAM · zephyrproject-rtos/zephyr · Discussion #36800 · GitHub&lt;/A&gt;. Altough a different device, it is still applicable for the RT1170.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Fri, 12 Sep 2025 21:03:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/Using-the-Link-Application-to-RAM-feature-in-MCUXpresso-for/m-p/2166990#M463</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-09-12T21:03:49Z</dc:date>
    </item>
  </channel>
</rss>