<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso for VSCodeのトピックRe: VS Code Extension import makefile project</title>
    <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1712566#M44</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222212"&gt;@mstahl&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;You already have noticed that linked files and folders are not supported (see as well &lt;A href="https://mcuoneclipse.com/2023/08/20/vs-code-importing-pre-v2-13-0-mcuxpresso-sdk-projects/" target="_blank"&gt;https://mcuoneclipse.com/2023/08/20/vs-code-importing-pre-v2-13-0-mcuxpresso-sdk-projects/&lt;/A&gt;), at least for now.&lt;/P&gt;&lt;P&gt;As for the project type: yes, it will not import make file projects through the NXP importer: it expects MCUXpresso IDE managed build/make projects, which are not the same as make projects.&lt;/P&gt;&lt;P&gt;What I did is using CMake projects (see &lt;A href="https://mcuoneclipse.com/2023/04/19/building-a-triumvirate-from-eclipse-cdt-to-cmake-cmd-and-visual-studio-code/" target="_blank"&gt;https://mcuoneclipse.com/2023/04/19/building-a-triumvirate-from-eclipse-cdt-to-cmake-cmd-and-visual-studio-code/&lt;/A&gt; ) and have them used with VSCode. You can do the same with make based projects too, the same way.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Aug 2023 18:00:29 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2023-08-28T18:00:29Z</dc:date>
    <item>
      <title>VS Code Extension import makefile project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1712383#M43</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;first of all I was amazed to hear that nxp also provides an extension for VS Code cause that is one of my favorite editors.&lt;/P&gt;&lt;P&gt;So I was trying to import an existing project into the MCUXpresso VS Code Extension.&lt;/P&gt;&lt;P&gt;The existing project uses makefiles (not CMake) as toolchain. The project is integrated into the MCUXpresso IDE v. 11.8 for Eclipse. It uses linked folders.&lt;/P&gt;&lt;P&gt;When trying to import that project into MCUXpresso VS Code, I got an error saying "Error: Invalid MCUXpresso IDE project directory: Cannot read properties of undefined (reading '0')". As I read elsewhere, linked folders are not yet supported so I removed the links and copied the sourcecode. This made the error go away, but the vsc code import wizard got another error saying&lt;/P&gt;&lt;P&gt;"Error: Invalid MCUXpresso IDE project directory: The description of the configuration could not be obtained"&lt;/P&gt;&lt;P&gt;I don't know if its possible to get some more info from vscode about what exactly went wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Might it be due to the fact that the project uses makefiles?&lt;/P&gt;&lt;P&gt;Might it be due to the fact that the project is not using the nxp configTools(pins, clocks, etc) at all? I thought about setting up the nxp configTools in eclipse and later deactivating everything in it because we dont need it. However, I seem to cannot set up nxp configTools in the first place.&lt;/P&gt;&lt;P&gt;I am thankful for any support&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 13:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1712383#M43</guid>
      <dc:creator>mstahl</dc:creator>
      <dc:date>2023-08-28T13:35:02Z</dc:date>
    </item>
    <item>
      <title>Re: VS Code Extension import makefile project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1712566#M44</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222212"&gt;@mstahl&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;You already have noticed that linked files and folders are not supported (see as well &lt;A href="https://mcuoneclipse.com/2023/08/20/vs-code-importing-pre-v2-13-0-mcuxpresso-sdk-projects/" target="_blank"&gt;https://mcuoneclipse.com/2023/08/20/vs-code-importing-pre-v2-13-0-mcuxpresso-sdk-projects/&lt;/A&gt;), at least for now.&lt;/P&gt;&lt;P&gt;As for the project type: yes, it will not import make file projects through the NXP importer: it expects MCUXpresso IDE managed build/make projects, which are not the same as make projects.&lt;/P&gt;&lt;P&gt;What I did is using CMake projects (see &lt;A href="https://mcuoneclipse.com/2023/04/19/building-a-triumvirate-from-eclipse-cdt-to-cmake-cmd-and-visual-studio-code/" target="_blank"&gt;https://mcuoneclipse.com/2023/04/19/building-a-triumvirate-from-eclipse-cdt-to-cmake-cmd-and-visual-studio-code/&lt;/A&gt; ) and have them used with VSCode. You can do the same with make based projects too, the same way.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Aug 2023 18:00:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1712566#M44</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-08-28T18:00:29Z</dc:date>
    </item>
    <item>
      <title>Re: VS Code Extension import makefile project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1713793#M46</link>
      <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;thanks a lot for your answer. I will try that and will come back to you.&lt;/P&gt;&lt;P&gt;Greets&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 07:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-for-VSCode/VS-Code-Extension-import-makefile-project/m-p/1713793#M46</guid>
      <dc:creator>mstahl</dc:creator>
      <dc:date>2023-08-30T07:11:09Z</dc:date>
    </item>
  </channel>
</rss>