<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDK中的主题 Task Aware Debugging</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Task-Aware-Debugging/m-p/807858#M991</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm debugging a FreeRTOS application using a Segger j-link debugger on a board that uses the K66 MCU.&amp;nbsp; I've found that stepping over an xTaskCreate results in the task code executing.&amp;nbsp; Is this a FreeRTOS question?&amp;nbsp; I thought I'd be able to create these tasks and that they would not execute until I start the task scheduler.&amp;nbsp; Any hints are greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 16:42:58 GMT</pubDate>
    <dc:creator>jeremyanderson</dc:creator>
    <dc:date>2018-08-01T16:42:58Z</dc:date>
    <item>
      <title>Task Aware Debugging</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Task-Aware-Debugging/m-p/807858#M991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm debugging a FreeRTOS application using a Segger j-link debugger on a board that uses the K66 MCU.&amp;nbsp; I've found that stepping over an xTaskCreate results in the task code executing.&amp;nbsp; Is this a FreeRTOS question?&amp;nbsp; I thought I'd be able to create these tasks and that they would not execute until I start the task scheduler.&amp;nbsp; Any hints are greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 16:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Task-Aware-Debugging/m-p/807858#M991</guid>
      <dc:creator>jeremyanderson</dc:creator>
      <dc:date>2018-08-01T16:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: Task Aware Debugging</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Task-Aware-Debugging/m-p/807859#M992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; tested the hello world demo with Frdm-k22 board.&amp;nbsp; I just added one print .&amp;nbsp; Then I debug with "step over",&amp;nbsp; I can see the hello world task is executed after vTaskStartScheduler. Please see below picture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79845i322E25D958B1BC8D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 08:18:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Task-Aware-Debugging/m-p/807859#M992</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-08-07T08:18:15Z</dc:date>
    </item>
  </channel>
</rss>