<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: Hello I can find the  SDK for the LPC1769... when is it going to be available ?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Hello-I-can-find-the-SDK-for-the-LPC1769-when-is-it-going-to-be/m-p/768802#M726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that there is no MCUXpresso SDK support for the LPC17 family. You need to use LPCOpen instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using MCUXpresso IDE, then an appropriateLPCOpen&amp;nbsp;package is included inside the Examples subdirectory of the IDE. See the IDE's User Guide for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information on LPCOpen, as well as packages for all toolchains, visit:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A class="link-titled" href="https://www.nxp.com/lpcopen" title="https://www.nxp.com/lpcopen"&gt;LPCOpen Libraries and Examples|NXP&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Apr 2018 10:10:09 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2018-04-26T10:10:09Z</dc:date>
    <item>
      <title>Hello I can find the  SDK for the LPC1769... when is it going to be available ?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Hello-I-can-find-the-SDK-for-the-LPC1769-when-is-it-going-to-be/m-p/768801#M725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying to download the sdk file for the LPC1769 but its not on the website.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 11:37:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Hello-I-can-find-the-SDK-for-the-LPC1769-when-is-it-going-to-be/m-p/768801#M725</guid>
      <dc:creator>giorgos_h4</dc:creator>
      <dc:date>2018-04-25T11:37:52Z</dc:date>
    </item>
    <item>
      <title>Re: Hello I can find the  SDK for the LPC1769... when is it going to be available ?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Hello-I-can-find-the-SDK-for-the-LPC1769-when-is-it-going-to-be/m-p/768802#M726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that there is no MCUXpresso SDK support for the LPC17 family. You need to use LPCOpen instead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using MCUXpresso IDE, then an appropriateLPCOpen&amp;nbsp;package is included inside the Examples subdirectory of the IDE. See the IDE's User Guide for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information on LPCOpen, as well as packages for all toolchains, visit:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A class="link-titled" href="https://www.nxp.com/lpcopen" title="https://www.nxp.com/lpcopen"&gt;LPCOpen Libraries and Examples|NXP&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 10:10:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Hello-I-can-find-the-SDK-for-the-LPC1769-when-is-it-going-to-be/m-p/768802#M726</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-04-26T10:10:09Z</dc:date>
    </item>
  </channel>
</rss>