<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need clarification on USB g_compositeDeviceConfigList.count in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Need-clarification-on-USB-g-compositeDeviceConfigList-count/m-p/757839#M615</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCUXpresso SDK USB Stack Composite Device User's Guide, section 4.2, says the config list count should be the number of classes in the composite device.&amp;nbsp; It shows as example MSD+CDC is 2 classes.&lt;/P&gt;&lt;P&gt;Shouldn't CDC+CDC be 1 class?&amp;nbsp; The SDK example twrk22f120m_dev_composite_cdc_vcom_cdc_vcom_freertos shows it as 2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 21:43:59 GMT</pubDate>
    <dc:creator>michaelhuslig</dc:creator>
    <dc:date>2018-06-06T21:43:59Z</dc:date>
    <item>
      <title>Need clarification on USB g_compositeDeviceConfigList.count</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Need-clarification-on-USB-g-compositeDeviceConfigList-count/m-p/757839#M615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCUXpresso SDK USB Stack Composite Device User's Guide, section 4.2, says the config list count should be the number of classes in the composite device.&amp;nbsp; It shows as example MSD+CDC is 2 classes.&lt;/P&gt;&lt;P&gt;Shouldn't CDC+CDC be 1 class?&amp;nbsp; The SDK example twrk22f120m_dev_composite_cdc_vcom_cdc_vcom_freertos shows it as 2.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 21:43:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Need-clarification-on-USB-g-compositeDeviceConfigList-count/m-p/757839#M615</guid>
      <dc:creator>michaelhuslig</dc:creator>
      <dc:date>2018-06-06T21:43:59Z</dc:date>
    </item>
    <item>
      <title>Re: Need clarification on USB g_compositeDeviceConfigList.count</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Need-clarification-on-USB-g-compositeDeviceConfigList-count/m-p/757840#M616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="13650" data-username="michaelhuslig" href="https://community.nxp.com/people/michaelhuslig"&gt;MICHAEl：&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CDC+CDC is two classes, usb stack will need allocate more memory. You can consider it as the count of classes rather than the type of&amp;nbsp; classes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jun 2018 08:52:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Need-clarification-on-USB-g-compositeDeviceConfigList-count/m-p/757840#M616</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-06-12T08:52:58Z</dc:date>
    </item>
  </channel>
</rss>