<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2389078#M5521</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have just started working with the &lt;STRONG&gt;RT1170 EVKB&lt;/STRONG&gt;&amp;nbsp;board and am trying to run the multicore &lt;STRONG&gt;Hello World&lt;/STRONG&gt;&amp;nbsp;example located in:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;boards/evkbmimxrt1170/multicore_examples/hello_world&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I am using the MCUXpresso SDK v26.03.00 (latest available version).&lt;/P&gt;&lt;P&gt;When I load the multicore example, the CM7 core hangs during startup, while the debugger shows that the CM4 core is running. The CM7 never reaches `main()`.&lt;/P&gt;&lt;P&gt;The fault status registers are:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cm7_hang.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/390938i46780A3E11248309/image-size/large?v=v2&amp;amp;px=999" role="button" title="cm7_hang.png" alt="cm7_hang.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To rule out an issue with the multicore example, I also tried running the standalone CM7 Hello World example, but it exhibits the same behavior. However, the standalone CM4 Hello World example runs correctly.&lt;/P&gt;&lt;P&gt;The board is an &lt;STRONG&gt;RT1170 EVKB&lt;/STRONG&gt; with the &lt;STRONG&gt;default jumper and DIP switch settings,&lt;/STRONG&gt; and I have not modified any hardware configuration.&lt;/P&gt;&lt;P&gt;Has anyone encountered this issue with SDK &lt;STRONG&gt;26.03.00&lt;/STRONG&gt; or the RT1170 EVKB? Is there any additional board configuration, boot setting, or debugger configuration required for the CM7 core?&lt;BR /&gt;&lt;BR /&gt;I also tested the previous SDK version (&lt;STRONG&gt;v2.13.0&lt;/STRONG&gt;), but I observed the same issue with the CM7 core.&lt;/P&gt;&lt;P&gt;Any suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 01 Jul 2026 10:43:20 GMT</pubDate>
    <dc:creator>FranklinOmo</dc:creator>
    <dc:date>2026-07-01T10:43:20Z</dc:date>
    <item>
      <title>RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2389078#M5521</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have just started working with the &lt;STRONG&gt;RT1170 EVKB&lt;/STRONG&gt;&amp;nbsp;board and am trying to run the multicore &lt;STRONG&gt;Hello World&lt;/STRONG&gt;&amp;nbsp;example located in:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;boards/evkbmimxrt1170/multicore_examples/hello_world&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I am using the MCUXpresso SDK v26.03.00 (latest available version).&lt;/P&gt;&lt;P&gt;When I load the multicore example, the CM7 core hangs during startup, while the debugger shows that the CM4 core is running. The CM7 never reaches `main()`.&lt;/P&gt;&lt;P&gt;The fault status registers are:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cm7_hang.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/390938i46780A3E11248309/image-size/large?v=v2&amp;amp;px=999" role="button" title="cm7_hang.png" alt="cm7_hang.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;To rule out an issue with the multicore example, I also tried running the standalone CM7 Hello World example, but it exhibits the same behavior. However, the standalone CM4 Hello World example runs correctly.&lt;/P&gt;&lt;P&gt;The board is an &lt;STRONG&gt;RT1170 EVKB&lt;/STRONG&gt; with the &lt;STRONG&gt;default jumper and DIP switch settings,&lt;/STRONG&gt; and I have not modified any hardware configuration.&lt;/P&gt;&lt;P&gt;Has anyone encountered this issue with SDK &lt;STRONG&gt;26.03.00&lt;/STRONG&gt; or the RT1170 EVKB? Is there any additional board configuration, boot setting, or debugger configuration required for the CM7 core?&lt;BR /&gt;&lt;BR /&gt;I also tested the previous SDK version (&lt;STRONG&gt;v2.13.0&lt;/STRONG&gt;), but I observed the same issue with the CM7 core.&lt;/P&gt;&lt;P&gt;Any suggestions would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 01 Jul 2026 10:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2389078#M5521</guid>
      <dc:creator>FranklinOmo</dc:creator>
      <dc:date>2026-07-01T10:43:20Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2389914#M5523</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264277"&gt;@FranklinOmo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you please share the schematic revision of your board? Additionally, to help simplify the review, could you send us a photo of the board?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 20:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2389914#M5523</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-07-02T20:07:57Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2390470#M5524</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231808"&gt;@Pablo_Ramos&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Here is an image of the board for your reference..&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="IMG_6141.jpg" style="width: 749px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/391236i5059870B4EF3C412/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_6141.jpg" alt="IMG_6141.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jul 2026 14:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2390470#M5524</guid>
      <dc:creator>FranklinOmo</dc:creator>
      <dc:date>2026-07-03T14:55:00Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170 EVKB Dual-Core Example: CM7 Hangs at Startup</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2390608#M5525</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264277"&gt;@FranklinOmo&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the picture of the board.&lt;/P&gt;
&lt;P&gt;Could you help me perform a mass erase of the board?&lt;/P&gt;
&lt;P&gt;You can find the steps for performing a mass erase using the SPT in the following document:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;RT board recovery for debugger connect issues&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you also help me test by updating the firmware?&lt;/P&gt;
&lt;P&gt;Instructions for updating the firmware can be found in Section 2.11, "On-board Debugger," of the MIMXRT1170-EVKB Board Hardware User Guide.&lt;/P&gt;
&lt;P&gt;Have you been able to successfully program and run a CM7 application before, or has this behavior been present since the board was first taken out of the box?&lt;/P&gt;
&lt;P&gt;If the problem persists, could you also try programming the device using the GUI Flash Tool or SPT?&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pablo&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jul 2026 20:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170-EVKB-Dual-Core-Example-CM7-Hangs-at-Startup/m-p/2390608#M5525</guid>
      <dc:creator>Pablo_Ramos</dc:creator>
      <dc:date>2026-07-03T20:59:17Z</dc:date>
    </item>
  </channel>
</rss>