<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Add USB Device CDC firmware support in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2336842#M5457</link>
    <description>&lt;P&gt;I am trying to add USB CDC VCOM device functionality to bare metal firmware running on an LPC55S26-based design. I have updated to the latest MCUXpresso IDE and SDK (with the USB Device middleware included). When I add the USB device to the project via the Peripherals tool and configure pins, clocks, etc I am left with two errors (both the same) and one warning as follows:&lt;/P&gt;&lt;P&gt;Error: "USB device CDC" driver is missing in the project.&lt;BR /&gt;Warning: An unsupported version of the USB Common Header in the toolchain/IDE project. Required: 2.8.0, actual: 2.12.1. The project might not compile correctly.&lt;/P&gt;&lt;P&gt;If I try to add the SDK component "USB Device CDC" I get a message that the component was not found in the SDK, however when I look in Available SDK Components it is present. Any suggestions much appreciated.&lt;/P&gt;</description>
    <pubDate>Sat, 21 Mar 2026 00:33:27 GMT</pubDate>
    <dc:creator>markpotts123</dc:creator>
    <dc:date>2026-03-21T00:33:27Z</dc:date>
    <item>
      <title>Add USB Device CDC firmware support</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2336842#M5457</link>
      <description>&lt;P&gt;I am trying to add USB CDC VCOM device functionality to bare metal firmware running on an LPC55S26-based design. I have updated to the latest MCUXpresso IDE and SDK (with the USB Device middleware included). When I add the USB device to the project via the Peripherals tool and configure pins, clocks, etc I am left with two errors (both the same) and one warning as follows:&lt;/P&gt;&lt;P&gt;Error: "USB device CDC" driver is missing in the project.&lt;BR /&gt;Warning: An unsupported version of the USB Common Header in the toolchain/IDE project. Required: 2.8.0, actual: 2.12.1. The project might not compile correctly.&lt;/P&gt;&lt;P&gt;If I try to add the SDK component "USB Device CDC" I get a message that the component was not found in the SDK, however when I look in Available SDK Components it is present. Any suggestions much appreciated.&lt;/P&gt;</description>
      <pubDate>Sat, 21 Mar 2026 00:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2336842#M5457</guid>
      <dc:creator>markpotts123</dc:creator>
      <dc:date>2026-03-21T00:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: Add USB Device CDC firmware support</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2337597#M5458</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240903"&gt;@markpotts123&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you for your post. I noticed that you also have a private case on the same topic, and I have already replied to you there. If you have any new updates, please feel free to respond in that case, and I will continue to support you.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Mon, 23 Mar 2026 11:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2337597#M5458</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-03-23T11:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: Add USB Device CDC firmware support</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2339423#M5460</link>
      <description>This turned out to be a mismatch between the IDE and SDK versions. Swirching to the latest versions fixed the symptom.</description>
      <pubDate>Wed, 25 Mar 2026 14:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Add-USB-Device-CDC-firmware-support/m-p/2339423#M5460</guid>
      <dc:creator>markpotts123</dc:creator>
      <dc:date>2026-03-25T14:42:58Z</dc:date>
    </item>
  </channel>
</rss>