<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックkw45 CAN Reception</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2253475#M5408</link>
    <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I am working with the &lt;LI-PRODUCT title="KW45B41Z-EVK" id="KW45B41Z-EVK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;board, and my goal is to implement CAN communication (both transmit and receive) on this BLE board&lt;/P&gt;&lt;P&gt;I have modified the flexcan_interrupt_transfer example by removing the dependency on a second node and attempted bidirectional communication. However, only the transmit functionality works correctly.&lt;/P&gt;&lt;P&gt;Additionally, when using the original flexcan_interrupt_transfer project and sending frames from a CAN traffic generator (with the same frame ID and CAN channel configured for reception), the board still does not receive any frames.&lt;/P&gt;&lt;P&gt;In both cases, the issue is that the board is unable to receive CAN frames. Could you help me identify the possible cause and guide me on resolving this?&lt;/P&gt;</description>
    <pubDate>Tue, 02 Dec 2025 20:54:33 GMT</pubDate>
    <dc:creator>paragl2</dc:creator>
    <dc:date>2025-12-02T20:54:33Z</dc:date>
    <item>
      <title>kw45 CAN Reception</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2253475#M5408</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;/P&gt;&lt;P&gt;I am working with the &lt;LI-PRODUCT title="KW45B41Z-EVK" id="KW45B41Z-EVK"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;board, and my goal is to implement CAN communication (both transmit and receive) on this BLE board&lt;/P&gt;&lt;P&gt;I have modified the flexcan_interrupt_transfer example by removing the dependency on a second node and attempted bidirectional communication. However, only the transmit functionality works correctly.&lt;/P&gt;&lt;P&gt;Additionally, when using the original flexcan_interrupt_transfer project and sending frames from a CAN traffic generator (with the same frame ID and CAN channel configured for reception), the board still does not receive any frames.&lt;/P&gt;&lt;P&gt;In both cases, the issue is that the board is unable to receive CAN frames. Could you help me identify the possible cause and guide me on resolving this?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Dec 2025 20:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2253475#M5408</guid>
      <dc:creator>paragl2</dc:creator>
      <dc:date>2025-12-02T20:54:33Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 CAN Reception</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2254361#M5411</link>
      <description>&lt;P&gt;Hello, Hello hope you are doing well,&lt;/P&gt;
&lt;P&gt;Could you help us describing the modifications implemented in the code?&lt;/P&gt;
&lt;P&gt;Could you help us confirm the following:&lt;/P&gt;
&lt;P&gt;Which SDK version are you using?&lt;/P&gt;
&lt;P&gt;Are you using 1 KW45B41Z-EVK board or 2 boards? Is the example without modifications working using 2 KW45B41Z-EVK as intended?&lt;/P&gt;
&lt;P&gt;Does the KW45B41Z-EVK has the 12V power supply on J9 to supply P5V_CAN?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share the terminal view when running the example? It would be highly appreciated&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Wed, 03 Dec 2025 16:45:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2254361#M5411</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-12-03T16:45:51Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 CAN Reception</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2255215#M5412</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Sorry to bother, first of all the issue is resolved. Seems like the issue with the traffic generator which I am using was faulty and not able to transmit frames on the bus.&lt;/P&gt;&lt;P&gt;Apart from that right now the rx is working properly. Thanks for the quick response though.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Dec 2025 10:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/kw45-CAN-Reception/m-p/2255215#M5412</guid>
      <dc:creator>paragl2</dc:creator>
      <dc:date>2025-12-04T10:26:49Z</dc:date>
    </item>
  </channel>
</rss>