<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックFiles missing from the MIMX9331 SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2174218#M5341</link>
    <description>&lt;P&gt;I started writing our firmware using a development board that had a MIMX9352 SoC. Our own hardware has a MIMX9331 SoC, so I downloaded the SDK (25.09) for that chip and updated the project files to use the correct SDK. This resulted in the build failing because the following files were missing:&lt;/P&gt;&lt;P&gt;components/uart/component_lpuart_adapter.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/all_lib_device.cmake&lt;BR /&gt;devices/MIMX9331/cmsis_drivers/driver_cmsis_lpi2c.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_CMSIS.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_startup.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_system.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_cache_xcache.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_clock.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_common.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_iomuxc.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_lpi2c_edma.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_lpuart.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_memory.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_rgpio.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/edma4/driver_edma4.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/debug_console_lite/utility_assert_lite.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utilities_misc_utilities.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utility_debug_console_lite.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utility_str.MIMX9331.cmake&lt;/P&gt;&lt;P&gt;The SDK for the MIMX9331 contains also the MIMX9352 files under devices, and the corresponding files for the 9352 exist there. As a workaround I've manually copied the missing files from the 9352 directory and renamed them (+ fixed the contents to refer to the 9331 when necessary).&lt;/P&gt;&lt;P&gt;Will the missing MIMX9331 files be added in an upcoming release?&lt;/P&gt;</description>
    <pubDate>Tue, 23 Sep 2025 10:03:12 GMT</pubDate>
    <dc:creator>TK6223</dc:creator>
    <dc:date>2025-09-23T10:03:12Z</dc:date>
    <item>
      <title>Files missing from the MIMX9331 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2174218#M5341</link>
      <description>&lt;P&gt;I started writing our firmware using a development board that had a MIMX9352 SoC. Our own hardware has a MIMX9331 SoC, so I downloaded the SDK (25.09) for that chip and updated the project files to use the correct SDK. This resulted in the build failing because the following files were missing:&lt;/P&gt;&lt;P&gt;components/uart/component_lpuart_adapter.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/all_lib_device.cmake&lt;BR /&gt;devices/MIMX9331/cmsis_drivers/driver_cmsis_lpi2c.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_CMSIS.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_startup.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/device_system.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_cache_xcache.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_clock.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_common.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_iomuxc.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_lpi2c_edma.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_lpuart.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_memory.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/driver_rgpio.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/drivers/edma4/driver_edma4.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/debug_console_lite/utility_assert_lite.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utilities_misc_utilities.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utility_debug_console_lite.MIMX9331.cmake&lt;BR /&gt;devices/MIMX9331/utilities/utility_str.MIMX9331.cmake&lt;/P&gt;&lt;P&gt;The SDK for the MIMX9331 contains also the MIMX9352 files under devices, and the corresponding files for the 9352 exist there. As a workaround I've manually copied the missing files from the 9352 directory and renamed them (+ fixed the contents to refer to the 9331 when necessary).&lt;/P&gt;&lt;P&gt;Will the missing MIMX9331 files be added in an upcoming release?&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 10:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2174218#M5341</guid>
      <dc:creator>TK6223</dc:creator>
      <dc:date>2025-09-23T10:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: Files missing from the MIMX9331 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2174324#M5343</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please take this appnote for differences between MX91 and MX93.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14012.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN14012.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 12:38:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2174324#M5343</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-09-23T12:38:30Z</dc:date>
    </item>
    <item>
      <title>Re: Files missing from the MIMX9331 SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2185811#M5361</link>
      <description>&lt;P&gt;Thanks for the reply! These are both i.MX93 chips so I don't see how the MX91 would be relevant here, but please correct me if I'm wrong.&lt;/P&gt;&lt;P&gt;And shouldn't there at least be the all_lib_device.cmake file with the corresponding configuration for the MIMX9331? I didn't check the peripherals related to each of the missing files, but for example the driver_clock, driver_common, driver_iomuxc and driver_rgpio files definitely sound like something that should be there.&lt;/P&gt;</description>
      <pubDate>Tue, 14 Oct 2025 13:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Files-missing-from-the-MIMX9331-SDK/m-p/2185811#M5361</guid>
      <dc:creator>TK6223</dc:creator>
      <dc:date>2025-10-14T13:18:13Z</dc:date>
    </item>
  </channel>
</rss>