<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDK中的主题 Re: Get_Version fails using PN7642</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2110332#M5198</link>
    <description>&lt;P&gt;Hey Fabian,&lt;/P&gt;&lt;P&gt;thanks for replying.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, it is an already personalized card. But Fsdi was 0x00 in my setup.&lt;/P&gt;&lt;P&gt;Now it works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you, best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
    <pubDate>Wed, 04 Jun 2025 09:55:32 GMT</pubDate>
    <dc:creator>MPEngineering</dc:creator>
    <dc:date>2025-06-04T09:55:32Z</dc:date>
    <item>
      <title>Get_Version fails using PN7642</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2109737#M5196</link>
      <description>&lt;P&gt;Hey there,&lt;/P&gt;&lt;P&gt;i have this problem that i can´t get a correct answer from&amp;nbsp;&lt;SPAN&gt;phalMfdfEVx_Sw_GetVersion() function. It´s a Mifare Defire EV2 card.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Overall everthing looks fine until the command:&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;NFC Lib Init Status: 0&lt;/P&gt;&lt;P&gt;HAL Init success: 0x0&lt;/P&gt;&lt;P&gt;PAL 14443p3a Init success: 0x0&lt;/P&gt;&lt;P&gt;PAL 14443p4 Init success: 0x0&lt;/P&gt;&lt;P&gt;PAL 14443p4a Init success: 0x0&lt;/P&gt;&lt;P&gt;PAL Mifare SW Init success: 0x0&lt;/P&gt;&lt;P&gt;HAL Mifare EVx Init success: 0x0&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Apply Protocol success: 0x0&lt;/P&gt;&lt;P&gt;Field ON success: 0x0&lt;/P&gt;&lt;P&gt;REQA success: 0x0&lt;/P&gt;&lt;P&gt;Anticollision successful: 0x0&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SAK: 0x20&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;RATS successful: 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;ATS Buffer: 0x6&lt;/P&gt;&lt;P&gt;CID Enable: 0x1&lt;/P&gt;&lt;P&gt;CID: 0x0&lt;/P&gt;&lt;P&gt;Nad Support: 0x0&lt;/P&gt;&lt;P&gt;FWI: 0x8&lt;/P&gt;&lt;P&gt;FSDI: 0x5&lt;/P&gt;&lt;P&gt;FSCI: 0x5&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when i want to ask which Version the card is i get:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;Get Version failed: 0x606&lt;/P&gt;&lt;P&gt;Get Version Out: 0x75&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a wrong Parameter or something else?&lt;/P&gt;&lt;P&gt;Do i have to load the ATS Parameters via &lt;SPAN&gt;phpalI14443p4_Sw_SetProtocol&lt;/SPAN&gt;() first?&lt;BR /&gt;Is it an authentication problem? Cause i thought its in Plain Mode and not a secured area in the card.&lt;BR /&gt;I think i´m at the point marked in the picture.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards and thanks for helping.&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 03 Jun 2025 18:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2109737#M5196</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-06-03T18:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: Get_Version fails using PN7642</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2109843#M5197</link>
      <description>&lt;P lang="en-US"&gt;Hello sir,&lt;/P&gt;
&lt;P lang="en-US"&gt;This is Fabian from customer support.&lt;/P&gt;
&lt;P lang="en-US"&gt;Is it possible that the MIFARE DESFire card could already be personalized?&lt;/P&gt;
&lt;P lang="en-US"&gt;In order to get the version of the DESFire card you only have to select Layer 4 with the following arguments:&lt;/P&gt;
&lt;P lang="en-US"&gt;Fsdi : 08&lt;/P&gt;
&lt;P lang="en-US"&gt;Cid: 00&lt;/P&gt;
&lt;P lang="en-US"&gt;Dri: 00&lt;/P&gt;
&lt;P lang="en-US"&gt;Dsi: 00&lt;/P&gt;
&lt;P lang="en-US"&gt;Please take a look at the following command exchange:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fabian_R_1-1748993351897.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341205i4B270BAE5D4754F1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Fabian_R_1-1748993351897.png" alt="Fabian_R_1-1748993351897.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I used a MIFARE DESFire EV3 but, the commands are exactly the same.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 23:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2109843#M5197</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2025-06-03T23:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: Get_Version fails using PN7642</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2110332#M5198</link>
      <description>&lt;P&gt;Hey Fabian,&lt;/P&gt;&lt;P&gt;thanks for replying.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, it is an already personalized card. But Fsdi was 0x00 in my setup.&lt;/P&gt;&lt;P&gt;Now it works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you, best regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 09:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Get-Version-fails-using-PN7642/m-p/2110332#M5198</guid>
      <dc:creator>MPEngineering</dc:creator>
      <dc:date>2025-06-04T09:55:32Z</dc:date>
    </item>
  </channel>
</rss>