<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: USB CDC CDC  composite Demo</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2017136#M5031</link>
    <description>&lt;P&gt;Hi Pavel, I have only specified the upper directory. I tested it with an EWARM V9.60.3. Full path is:&lt;BR /&gt;\SDK_2_16_000_EVK-MIMXRT1064\boards\evkmimxrt1064\usb_examples\usb_device_composite_cdc_vcom_cdc_vcom\bm\iar\dev_composite_cdc_vcom_cdc_vcom_bm.eww\dev_composite_cdc_vcom_cdc_vcom_bm.eww.&lt;BR /&gt;The same error occurs with the “Lite” and “FreeRTOS” variants.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Dec 2024 10:05:28 GMT</pubDate>
    <dc:creator>johannzimmerman</dc:creator>
    <dc:date>2024-12-19T10:05:28Z</dc:date>
    <item>
      <title>USB CDC CDC  composite Demo</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2015304#M5022</link>
      <description>&lt;P&gt;IMXRT1064 SDK_2_16&lt;/P&gt;&lt;P&gt;usb_device_composite_cdc_vcom_cdc_vcom Example shows the tool UsbTreeView.exe&lt;BR /&gt;tool displays an error: ”&lt;BR /&gt;----------------- Device Qualifier Descriptor -----------------&lt;BR /&gt;Error : ERROR_GEN_FAILURE (*!*ERROR USB 2.0 HighSpeed devices must provide a Device Qualifier Descriptor)”&lt;/P&gt;&lt;P&gt;The example of “usbx_device_composite_cdc_acm_cdc_acm” does not show this error.&lt;/P&gt;&lt;P&gt;Seems that in the first example a descriptor type is missing or?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 12:36:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2015304#M5022</guid>
      <dc:creator>johannzimmerman</dc:creator>
      <dc:date>2024-12-17T12:36:24Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC CDC  composite Demo</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2016401#M5027</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I could not find the example "&lt;SPAN&gt;&lt;STRONG&gt;usb_device_composite_cdc_vcom_cdc_vcom&lt;/STRONG&gt;"&amp;nbsp;&lt;/SPAN&gt;on the SDK v2.16, could you confirm the name of this? I find the next.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1734554026986.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/316549iC825C6BA731D9621/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1734554026986.png" alt="Pavel_Hernandez_0-1734554026986.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 20:34:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2016401#M5027</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-18T20:34:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC CDC  composite Demo</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2017136#M5031</link>
      <description>&lt;P&gt;Hi Pavel, I have only specified the upper directory. I tested it with an EWARM V9.60.3. Full path is:&lt;BR /&gt;\SDK_2_16_000_EVK-MIMXRT1064\boards\evkmimxrt1064\usb_examples\usb_device_composite_cdc_vcom_cdc_vcom\bm\iar\dev_composite_cdc_vcom_cdc_vcom_bm.eww\dev_composite_cdc_vcom_cdc_vcom_bm.eww.&lt;BR /&gt;The same error occurs with the “Lite” and “FreeRTOS” variants.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 10:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2017136#M5031</guid>
      <dc:creator>johannzimmerman</dc:creator>
      <dc:date>2024-12-19T10:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC CDC  composite Demo</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2018090#M5033</link>
      <description>&lt;P&gt;Hello, thanks for your information I replayed the behavior, let me escalate to get more details about it. I want to add to the USB on the EVK does not have any certification is only for evaluation porpoise.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 22:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2018090#M5033</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-20T22:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC CDC  composite Demo</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2021464#M5034</link>
      <description>&lt;P&gt;Hello, this is the answerback: The device_qualifier_descriptor is used to illustrate the configurations that the different speed of this device, but this only needed when the configurations have difference between different speed.&lt;/P&gt;
&lt;P&gt;For this demo, I think there is no need for this descriptor, it can work both on High speed and Full speed.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jan 2025 23:35:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/USB-CDC-CDC-composite-Demo/m-p/2021464#M5034</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2025-01-02T23:35:46Z</dc:date>
    </item>
  </channel>
</rss>