<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: RT1170EVKB USB-RNDIS automatic recognition</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170EVKB-USB-RNDIS-automatic-recognition/m-p/1962528#M4951</link>
    <description>&lt;P&gt;I have confirmed that the Ethernet device is automatically recognized on UBUNTU.&lt;/P&gt;&lt;P&gt;I would like to cancel this question.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
    <pubDate>Thu, 26 Sep 2024 08:43:52 GMT</pubDate>
    <dc:creator>seobi</dc:creator>
    <dc:date>2024-09-26T08:43:52Z</dc:date>
    <item>
      <title>RT1170EVKB USB-RNDIS automatic recognition</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170EVKB-USB-RNDIS-automatic-recognition/m-p/1961563#M4950</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hi, I successfully communicated with a Windows PC using the VNIC sample and lwIP sample on the RT1170EVKB.&lt;/P&gt;&lt;P&gt;However, to enable communication on the Windows PC, I had to install the "fsl_rndis.inf" file for the Ethernet device to be created.&lt;/P&gt;&lt;P&gt;The issue is that this works on Windows, but I'm not sure how to use the RNDIS functionality on Linux (such as Ubuntu).&lt;/P&gt;&lt;P&gt;I hope RNDIS will be automatically recognized by all operating systems.&lt;/P&gt;&lt;P&gt;Is there a way to enable RNDIS mode on operating systems other than Windows, such as Linux?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 08:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170EVKB-USB-RNDIS-automatic-recognition/m-p/1961563#M4950</guid>
      <dc:creator>seobi</dc:creator>
      <dc:date>2024-09-25T08:52:22Z</dc:date>
    </item>
    <item>
      <title>Re: RT1170EVKB USB-RNDIS automatic recognition</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170EVKB-USB-RNDIS-automatic-recognition/m-p/1962528#M4951</link>
      <description>&lt;P&gt;I have confirmed that the Ethernet device is automatically recognized on UBUNTU.&lt;/P&gt;&lt;P&gt;I would like to cancel this question.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Thu, 26 Sep 2024 08:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1170EVKB-USB-RNDIS-automatic-recognition/m-p/1962528#M4951</guid>
      <dc:creator>seobi</dc:creator>
      <dc:date>2024-09-26T08:43:52Z</dc:date>
    </item>
  </channel>
</rss>