<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: flexio camera in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/flexio-camera/m-p/1950374#M4926</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228348"&gt;@seobi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.&lt;/P&gt;
&lt;P&gt;2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Mon, 09 Sep 2024 22:48:58 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-09-09T22:48:58Z</dc:date>
    <item>
      <title>flexio camera</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/flexio-camera/m-p/1945760#M4912</link>
      <description>&lt;P&gt;Hi, We are planning to use a parallel camera with FlexIO on the EVKBRT1170.&lt;/P&gt;&lt;P&gt;Referring to the RT1010 sample, we have two questions during the implementation:&lt;/P&gt;&lt;P&gt;1. The PCLK on the RT1010 is said to support up to 20MHz.&amp;nbsp;&lt;SPAN&gt;How much is supported in the case of the RT1170? I couldn't find this information in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;2. The sample for the RT1010 is for 8-bit data, but in our case, we need to use 16-bit data. Is it possible to obtain a sample for this? If not, could you guide us on what needs to be modified?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Tue, 03 Sep 2024 02:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/flexio-camera/m-p/1945760#M4912</guid>
      <dc:creator>seobi</dc:creator>
      <dc:date>2024-09-03T02:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: flexio camera</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/flexio-camera/m-p/1950374#M4926</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228348"&gt;@seobi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.&lt;/P&gt;
&lt;P&gt;2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Sep 2024 22:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/flexio-camera/m-p/1950374#M4926</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-09-09T22:48:58Z</dc:date>
    </item>
  </channel>
</rss>