<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: Use multiple USB composite with multiple CDC VCOM</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Use-multiple-USB-composite-with-multiple-CDC-VCOM/m-p/1875777#M4785</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65478"&gt;@biafra&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid that the SDK does not support triple CDC VCOM interfaces. I apologize for the inconvenience.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
    <pubDate>Mon, 27 May 2024 23:20:54 GMT</pubDate>
    <dc:creator>EdwinHz</dc:creator>
    <dc:date>2024-05-27T23:20:54Z</dc:date>
    <item>
      <title>Use multiple USB composite with multiple CDC VCOM</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Use-multiple-USB-composite-with-multiple-CDC-VCOM/m-p/1874455#M4784</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a custom board based on RT1064, using MCUXpresso 11.9.1 and SDK 2.13.0.&lt;/P&gt;&lt;P&gt;Based on the example provided in the SDK, I use a usb composite device&amp;nbsp;&lt;SPAN&gt;with dual CDC &lt;/SPAN&gt;&lt;SPAN&gt;vcom interface, and it's working fine.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Due to some extra needs, I extended the&amp;nbsp;usb composite device to act as a triple&amp;nbsp;&lt;SPAN&gt;CDC &lt;/SPAN&gt;&lt;SPAN&gt;vcom interface: I modified the sources adding&amp;nbsp;everything necessary (I've defined endpoints, strings, structures, ...). The composite device is enumerated correctly and the first two interfaces are working fine, but the third one isn't working: no data is tranferred to/from the connected host.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any limitation on this scenario?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Many thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Biafra&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 08:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Use-multiple-USB-composite-with-multiple-CDC-VCOM/m-p/1874455#M4784</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2024-05-24T08:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: Use multiple USB composite with multiple CDC VCOM</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Use-multiple-USB-composite-with-multiple-CDC-VCOM/m-p/1875777#M4785</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65478"&gt;@biafra&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm afraid that the SDK does not support triple CDC VCOM interfaces. I apologize for the inconvenience.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 23:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Use-multiple-USB-composite-with-multiple-CDC-VCOM/m-p/1875777#M4785</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-05-27T23:20:54Z</dc:date>
    </item>
  </channel>
</rss>