<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Failing High Speed detection handshake in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failing-High-Speed-detection-handshake/m-p/1813852#M4620</link>
    <description>&lt;P&gt;In Errata Sheet "LPC55S2x_LPC552x_ES", Rev. 2.5 — 19 December 2023, problem 3.5 USB.3: mentions a scenario where a High Speed device is connected to a Full Speed hub.&lt;/P&gt;&lt;P&gt;We have a Full Speed device, connected to a High Speed hub, and are facing an intermittent issue establishing connection from device to host. we are observing that when we do a sequence of rapid disconnect and reconnect, we sometimes are unsuccessful in reconnecting device to host.&lt;/P&gt;&lt;P&gt;Reading through 3.5 USB.3: in the Errata Sheet, we have found, implemented and tested option 2 as listed in the Errata Sheet, and found that it solves our issue reconnecting to host?&lt;/P&gt;&lt;P&gt;Can you confirm that this is the correct way for solving our issue, even though we are working with a scenario, where the speed of the hub used and device involded are inverted?&lt;/P&gt;</description>
    <pubDate>Thu, 22 Feb 2024 14:30:04 GMT</pubDate>
    <dc:creator>STPS</dc:creator>
    <dc:date>2024-02-22T14:30:04Z</dc:date>
    <item>
      <title>Failing High Speed detection handshake</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failing-High-Speed-detection-handshake/m-p/1813852#M4620</link>
      <description>&lt;P&gt;In Errata Sheet "LPC55S2x_LPC552x_ES", Rev. 2.5 — 19 December 2023, problem 3.5 USB.3: mentions a scenario where a High Speed device is connected to a Full Speed hub.&lt;/P&gt;&lt;P&gt;We have a Full Speed device, connected to a High Speed hub, and are facing an intermittent issue establishing connection from device to host. we are observing that when we do a sequence of rapid disconnect and reconnect, we sometimes are unsuccessful in reconnecting device to host.&lt;/P&gt;&lt;P&gt;Reading through 3.5 USB.3: in the Errata Sheet, we have found, implemented and tested option 2 as listed in the Errata Sheet, and found that it solves our issue reconnecting to host?&lt;/P&gt;&lt;P&gt;Can you confirm that this is the correct way for solving our issue, even though we are working with a scenario, where the speed of the hub used and device involded are inverted?&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 14:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failing-High-Speed-detection-handshake/m-p/1813852#M4620</guid>
      <dc:creator>STPS</dc:creator>
      <dc:date>2024-02-22T14:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: Failing High Speed detection handshake</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failing-High-Speed-detection-handshake/m-p/1815248#M4623</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229895"&gt;@STPS&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think you can first test with the method. If still have issue, can contact us.&lt;/P&gt;
&lt;P&gt;BTW, whether can config your HUB&amp;nbsp; to FS speed.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 06:32:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failing-High-Speed-detection-handshake/m-p/1815248#M4623</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2024-02-26T06:32:40Z</dc:date>
    </item>
  </channel>
</rss>