<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC55S06 How do you Map Capture Inputs to CTimer Channels in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1747244#M4522</link>
    <description>&lt;P&gt;I saw that diagram, but unfortunately that chapter does not indicate how to map them in code.&amp;nbsp; Nor does the IOCON chapter.&amp;nbsp; However, diving deeper into the manual, the chapter that does provide information on how to map them is the INPUTMUX chapter (chapter 18). At least that chapter, along with the fsl_inputmux driver source, I was able to decipher how to get a CTIMER_INPxx mapped to a specific timer and channel (test case of 1, but I think I have figured it out &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Oct 2023 16:29:05 GMT</pubDate>
    <dc:creator>ttahut</dc:creator>
    <dc:date>2023-10-26T16:29:05Z</dc:date>
    <item>
      <title>LPC55S06 How do you Map Capture Inputs to CTimer Channels</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1746111#M4517</link>
      <description>&lt;P&gt;I want to use a CTimer on the LPC55S06 in timer mode and capture a signal on a Capture input.&amp;nbsp; The users manual (and data sheet for that matter) show capture inputs as CTIMER_INP0 - CTIMER_INP16 in the pin mux tables.&amp;nbsp; The CTIMER section of the manual indicates "&lt;EM&gt;The capture signal is generated by one&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;of the pins with a capture function. Each capture signal is connected to one capture&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;channel of the timer&lt;/EM&gt;."&amp;nbsp; I do not see a way in the register descriptions to map a CTIMER_INPxx to a specific CTIMER and channel.&amp;nbsp; Are they just mapped sequentially so for example CTIMER_INP0 - CTIMER_INP3 are on CTIMER0 channels 0-3 respectively?&amp;nbsp; And following that, CTIMER_INP9 would be on CTIMER2 channel 1.&amp;nbsp; Or am I missing something in the manual?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Oct 2023 16:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1746111#M4517</guid>
      <dc:creator>ttahut</dc:creator>
      <dc:date>2023-10-25T16:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S06 How do you Map Capture Inputs to CTimer Channels</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1746867#M4520</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/3640"&gt;@ttahut&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;They can flexible to configuration, you can refer to the fig78:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1698311948782.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/246921i97A8683896287C24/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1698311948782.png" alt="Alice_Yang_0-1698311948782.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_0-1698311948782.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For example,&amp;nbsp;&lt;SPAN&gt;CTIMER_INP9&amp;nbsp;can configured to CTIMER0 capture0, also can configured to CTIMER2 capture 3. You can use config tool to check:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_1-1698312110491.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/246923iFC462BF746304807/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_1-1698312110491.png" alt="Alice_Yang_1-1698312110491.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Alice_Yang_1-1698312110491.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Oct 2023 09:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1746867#M4520</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2023-10-26T09:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S06 How do you Map Capture Inputs to CTimer Channels</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1747244#M4522</link>
      <description>&lt;P&gt;I saw that diagram, but unfortunately that chapter does not indicate how to map them in code.&amp;nbsp; Nor does the IOCON chapter.&amp;nbsp; However, diving deeper into the manual, the chapter that does provide information on how to map them is the INPUTMUX chapter (chapter 18). At least that chapter, along with the fsl_inputmux driver source, I was able to decipher how to get a CTIMER_INPxx mapped to a specific timer and channel (test case of 1, but I think I have figured it out &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Oct 2023 16:29:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/LPC55S06-How-do-you-Map-Capture-Inputs-to-CTimer-Channels/m-p/1747244#M4522</guid>
      <dc:creator>ttahut</dc:creator>
      <dc:date>2023-10-26T16:29:05Z</dc:date>
    </item>
  </channel>
</rss>