<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What console is the default PRINTF line in projects printing to? in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/What-console-is-the-default-PRINTF-line-in-projects-printing-to/m-p/1728228#M4483</link>
    <description>&lt;P&gt;Hello, I've just started using MCUXpresso, so I'm sorry if this question has an obvious answer.&lt;/P&gt;&lt;P&gt;When I use the SDK Wizard to create a project for my board (FRDM-KL25Z) using the default settings, the main function always contains the line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;PRINTF("Hello World\n");&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I need to do some debugging and this function seems useful for that purpose, but I can't figure out what console this function is printing to.&lt;/P&gt;</description>
    <pubDate>Fri, 22 Sep 2023 18:09:40 GMT</pubDate>
    <dc:creator>MelonM</dc:creator>
    <dc:date>2023-09-22T18:09:40Z</dc:date>
    <item>
      <title>What console is the default PRINTF line in projects printing to?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/What-console-is-the-default-PRINTF-line-in-projects-printing-to/m-p/1728228#M4483</link>
      <description>&lt;P&gt;Hello, I've just started using MCUXpresso, so I'm sorry if this question has an obvious answer.&lt;/P&gt;&lt;P&gt;When I use the SDK Wizard to create a project for my board (FRDM-KL25Z) using the default settings, the main function always contains the line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;PRINTF("Hello World\n");&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;I need to do some debugging and this function seems useful for that purpose, but I can't figure out what console this function is printing to.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 18:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/What-console-is-the-default-PRINTF-line-in-projects-printing-to/m-p/1728228#M4483</guid>
      <dc:creator>MelonM</dc:creator>
      <dc:date>2023-09-22T18:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: What console is the default PRINTF line in projects printing to?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/What-console-is-the-default-PRINTF-line-in-projects-printing-to/m-p/1729226#M4484</link>
      <description>&lt;P&gt;Hello, I suggest reviewing the device COM available on the device manager then you need to use software to see the message like tera term or other.&lt;/P&gt;&lt;P&gt;Let me know if you have more doubts.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 01:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/What-console-is-the-default-PRINTF-line-in-projects-printing-to/m-p/1729226#M4484</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2023-09-26T01:17:50Z</dc:date>
    </item>
  </channel>
</rss>