<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックIMX8MP Cortex M7 FreeRTOS FlexCAN Driver</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1628477#M4278</link>
    <description>&lt;P&gt;I'm currently working on a project using the IMX8MP (with the Cortex-M7), specifically, the processor is&amp;nbsp;&lt;SPAN&gt;MIMX8ML8CVNKZ. I need to use FlexCAN in FreeRTOS and I see that there is a bare metal driver (and examples) but there is no FreeRTOS/CMSIS driver in the SDK (as of the latest version v2.13.0). Are there any patches or notes (or even already ported FlexCAN drivers) that I could use? If not, could you point me in the right direction for porting the FlexCAN driver for FreeRTOS?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I did see another post with a similar question on the forum from 4 years ago where NXP said it's on their roadmap to add but there's been no update since:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/FlexCAN-FreeRTOS-Driver/m-p/857383/highlight/true#M1217" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MCUXpresso-SDK/FlexCAN-FreeRTOS-Driver/m-p/857383/highlight/true#M1217&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 07 Apr 2023 10:52:47 GMT</pubDate>
    <dc:creator>daharingwitekio</dc:creator>
    <dc:date>2023-04-07T10:52:47Z</dc:date>
    <item>
      <title>IMX8MP Cortex M7 FreeRTOS FlexCAN Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1628477#M4278</link>
      <description>&lt;P&gt;I'm currently working on a project using the IMX8MP (with the Cortex-M7), specifically, the processor is&amp;nbsp;&lt;SPAN&gt;MIMX8ML8CVNKZ. I need to use FlexCAN in FreeRTOS and I see that there is a bare metal driver (and examples) but there is no FreeRTOS/CMSIS driver in the SDK (as of the latest version v2.13.0). Are there any patches or notes (or even already ported FlexCAN drivers) that I could use? If not, could you point me in the right direction for porting the FlexCAN driver for FreeRTOS?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I did see another post with a similar question on the forum from 4 years ago where NXP said it's on their roadmap to add but there's been no update since:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/FlexCAN-FreeRTOS-Driver/m-p/857383/highlight/true#M1217" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/MCUXpresso-SDK/FlexCAN-FreeRTOS-Driver/m-p/857383/highlight/true#M1217&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 10:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1628477#M4278</guid>
      <dc:creator>daharingwitekio</dc:creator>
      <dc:date>2023-04-07T10:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Cortex M7 FreeRTOS FlexCAN Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1629701#M4281</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210051"&gt;@daharingwitekio&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It can be ported from other platforms. For example, there is a flex_can driver in the SDK package of i.MX RT1170. It should be a faster way to try to use it on the i.MX8MP SDK.&amp;nbsp;After consulting the R&amp;amp;D team, so far,&amp;nbsp;they have no plan to add it to the SDK release.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Apr 2023 10:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1629701#M4281</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-04-07T10:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Cortex M7 FreeRTOS FlexCAN Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1642455#M4304</link>
      <description>&lt;P&gt;When you say there's a flexcan driver for i.MX RT1170, do you mean there's a bare metal one or a freertos one (I don't need a bare metal one as the i.MX8M P already has bare metal flexcan drivers)? I downloaded a few SDK's for the RT1170 but didn't see any freertos flexcan drivers. Maybe I'm looking in the wrong spot? Could you point me to the specific rt1170 processor I should download the SDK for to find sample flexcan freertos drivers?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 21:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1642455#M4304</guid>
      <dc:creator>daharingwitekio</dc:creator>
      <dc:date>2023-04-28T21:03:39Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Cortex M7 FreeRTOS FlexCAN Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1644086#M4305</link>
      <description>&lt;P&gt;There is no FlexCAN driver for FreeRTOS for now.&amp;nbsp;&lt;SPAN class=""&gt;I have consulted with R&amp;amp;D, if you need to add FlexCAN driver in SDK for FreeRTOS, you may need to make a request to marketing, then R&amp;amp;D will add it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 May 2023 23:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/IMX8MP-Cortex-M7-FreeRTOS-FlexCAN-Driver/m-p/1644086#M4305</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-05-03T23:24:54Z</dc:date>
    </item>
  </channel>
</rss>