<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Dual channel Rpmsg in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Dual-channel-Rpmsg/m-p/1573775#M4063</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project using a custom board based on imx8m mini. I have to desing the communication between A53 cores and M4 core using rpmsg.&lt;BR /&gt;I already saw the rpmsg ping pong example and it's working fine on my board.&lt;/P&gt;&lt;P&gt;To avoid polling mechanism on both sides, I'd want to have the A53 cores waiting for a message from the M4 core and at the same time the M4 core waiting for a message from the A53 cores on a different channel.&lt;BR /&gt;How can this be achived?&lt;BR /&gt;Do I have to duplicate the instructions between rpmsg_lite_remote_init() and rpmsg_ns_announce() in the main_remote.c source file of the rpmsg ping pong example?&lt;BR /&gt;Or is there a better solution?&lt;/P&gt;&lt;P&gt;Many thanks&lt;BR /&gt;Biafra&lt;/P&gt;</description>
    <pubDate>Thu, 22 Dec 2022 13:56:27 GMT</pubDate>
    <dc:creator>biafra</dc:creator>
    <dc:date>2022-12-22T13:56:27Z</dc:date>
    <item>
      <title>Dual channel Rpmsg</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Dual-channel-Rpmsg/m-p/1573775#M4063</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project using a custom board based on imx8m mini. I have to desing the communication between A53 cores and M4 core using rpmsg.&lt;BR /&gt;I already saw the rpmsg ping pong example and it's working fine on my board.&lt;/P&gt;&lt;P&gt;To avoid polling mechanism on both sides, I'd want to have the A53 cores waiting for a message from the M4 core and at the same time the M4 core waiting for a message from the A53 cores on a different channel.&lt;BR /&gt;How can this be achived?&lt;BR /&gt;Do I have to duplicate the instructions between rpmsg_lite_remote_init() and rpmsg_ns_announce() in the main_remote.c source file of the rpmsg ping pong example?&lt;BR /&gt;Or is there a better solution?&lt;/P&gt;&lt;P&gt;Many thanks&lt;BR /&gt;Biafra&lt;/P&gt;</description>
      <pubDate>Thu, 22 Dec 2022 13:56:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Dual-channel-Rpmsg/m-p/1573775#M4063</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2022-12-22T13:56:27Z</dc:date>
    </item>
    <item>
      <title>Re: Dual channel Rpmsg</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Dual-channel-Rpmsg/m-p/1575222#M4087</link>
      <description>&lt;DIV&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65478"&gt;@biafra&lt;/a&gt;&amp;nbsp;,&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;I hope you are doing well.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;you can create multiple&amp;nbsp;channels in rpmsg lite.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;you can follow the below suggestions to create multiple&amp;nbsp;channels&amp;nbsp;in rpmsg-lite:&lt;/DIV&gt;
&lt;DIV&gt;- need separate vdev rings allocations(VDEVn_VRING_BASE) in board.h and RL_PLATFORM_IMX8MN_M7_USER_&lt;WBR /&gt;LINK_ID at /middleware/multicore/rpmsg_&lt;WBR /&gt;lite/lib/include/platform/&lt;WBR /&gt;imx8mn_m7/rpmsg_platform.h&lt;/DIV&gt;
&lt;DIV&gt;- need a separate definition&amp;nbsp;for&amp;nbsp;LOCAL_EPT_ADDR,&lt;WBR /&gt;&amp;nbsp;RPMSG_LITE_SHMEM_BASE, RPMSG_LITE_LINK_ID.&lt;/DIV&gt;
&lt;DIV&gt;-&amp;nbsp; have to make multiple calls to&amp;nbsp;rpmsg_lite_remote_init(),&lt;WBR /&gt;rpmsg_lite_wait_for_link_up(),&lt;WBR /&gt;rpmsg_queue_create(),rpmsg_&lt;WBR /&gt;lite_create_ept(),rpmsg_ns_&lt;WBR /&gt;announce().&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;Thanks &amp;amp; Regards&lt;/DIV&gt;
&lt;DIV&gt;Sanket Parekh&lt;/DIV&gt;</description>
      <pubDate>Wed, 28 Dec 2022 13:59:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Dual-channel-Rpmsg/m-p/1575222#M4087</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2022-12-28T13:59:55Z</dc:date>
    </item>
  </channel>
</rss>