<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDK中的主题 Re: rt1050 RTC cannot start.</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503878#M3856</link>
    <description>&lt;P&gt;Hello, we have same issue on imx7ulp. When jtag is attached or when linux is in suspended state (sudo systemctl suspend) and then wdog reset action happen.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Aug 2022 09:47:07 GMT</pubDate>
    <dc:creator>cervenka</dc:creator>
    <dc:date>2022-08-10T09:47:07Z</dc:date>
    <item>
      <title>rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1313153#M3280</link>
      <description>&lt;P&gt;Run&amp;nbsp;evkbimxrt1050_snvs_hp_rtc demo application on our RT1050 board. the application entries to the dead loop here:&lt;/P&gt;&lt;P&gt;static inline void SNVS_HP_RTC_StartTimer(SNVS_Type *base)&lt;BR /&gt;{&lt;BR /&gt;base-&amp;gt;HPCR |= SNVS_HPCR_RTC_EN_MASK;&lt;BR /&gt;while (0U == (base-&amp;gt;HPCR &amp;amp; SNVS_HPCR_RTC_EN_MASK))&lt;BR /&gt;{&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;we cannot start the HP_RTC, we retry the&amp;nbsp;evkbimxrt1050_snvs_lp_rtc demo application, the&amp;nbsp;SNVS_LP_SRTC_StartTimer(SNVS) has the same deep loop on our RT1050 board.&lt;/P&gt;&lt;P&gt;the two RTC demo runs ok on the RT1050 EVB board. we compare the 32K clock between the RT1050 evb and our board, the 32k is ok.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Our board has not backup battery, the VCC_SNVS_IN has special LDO, the LDO is always on when the power supply on.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 09:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1313153#M3280</guid>
      <dc:creator>meitifire</dc:creator>
      <dc:date>2021-07-26T09:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1313505#M3285</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;According to your statement, I guess the phenomenon is related to the hardware, so I was wondering if you can share the schematic of your custom board.&lt;BR /&gt;Looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 02:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1313505#M3285</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2021-07-27T02:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503332#M3854</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189502"&gt;@meitifire&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just wondering whether you ever found a resolution to this please?&lt;/P&gt;&lt;P&gt;I am working on a project where we've seen the same fault and can't find a reason for it.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 13:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503332#M3854</guid>
      <dc:creator>Steve23</dc:creator>
      <dc:date>2022-08-09T13:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503878#M3856</link>
      <description>&lt;P&gt;Hello, we have same issue on imx7ulp. When jtag is attached or when linux is in suspended state (sudo systemctl suspend) and then wdog reset action happen.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 09:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503878#M3856</guid>
      <dc:creator>cervenka</dc:creator>
      <dc:date>2022-08-10T09:47:07Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503893#M3858</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes we also only see the problem when connected with JTAG. I've raised a new question here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/RT1062-SNVS-HP-RTC-StartTimer-call-does-not-return/m-p/1503889#M3857" target="_blank"&gt;RT1062 SNVS_HP_RTC_StartTimer() call does not retu... - NXP Community&lt;/A&gt;&amp;nbsp;because I don't think NXP monitor old threads.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Aug 2022 10:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1503893#M3858</guid>
      <dc:creator>Steve23</dc:creator>
      <dc:date>2022-08-10T10:10:36Z</dc:date>
    </item>
    <item>
      <title>Re: rt1050 RTC cannot start.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1527411#M3922</link>
      <description>yeh we are having the exact same issue on the imx7ulp evk as well, has a solution been found yet?</description>
      <pubDate>Fri, 23 Sep 2022 13:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/rt1050-RTC-cannot-start/m-p/1527411#M3922</guid>
      <dc:creator>Jonny_T</dc:creator>
      <dc:date>2022-09-23T13:45:48Z</dc:date>
    </item>
  </channel>
</rss>