<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KW41Z With SDK2.2.3 HardFault in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367443#M3418</link>
    <description>&lt;P&gt;Dear sirs,&lt;/P&gt;&lt;P&gt;While trying to use the SDK example&amp;nbsp;frdmkw41z_wireless_examples_thread_end_device_freertos (but it happen also with router eligible thread end device) I can join the device to the thread network created with Openthread but every time I try to send something pushing a button the KW41Z enter in an hard fault condition.&lt;/P&gt;&lt;P&gt;Querying the board though serial port works.&lt;/P&gt;&lt;P&gt;I'm not able to debug the Hardfault cause it point to strange stack position.&lt;/P&gt;&lt;P&gt;Does anyone have some advice?&lt;/P&gt;&lt;P&gt;Best&lt;/P&gt;&lt;P&gt;Alessio&lt;/P&gt;</description>
    <pubDate>Fri, 05 Nov 2021 16:55:06 GMT</pubDate>
    <dc:creator>agalliazzo</dc:creator>
    <dc:date>2021-11-05T16:55:06Z</dc:date>
    <item>
      <title>KW41Z With SDK2.2.3 HardFault</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367443#M3418</link>
      <description>&lt;P&gt;Dear sirs,&lt;/P&gt;&lt;P&gt;While trying to use the SDK example&amp;nbsp;frdmkw41z_wireless_examples_thread_end_device_freertos (but it happen also with router eligible thread end device) I can join the device to the thread network created with Openthread but every time I try to send something pushing a button the KW41Z enter in an hard fault condition.&lt;/P&gt;&lt;P&gt;Querying the board though serial port works.&lt;/P&gt;&lt;P&gt;I'm not able to debug the Hardfault cause it point to strange stack position.&lt;/P&gt;&lt;P&gt;Does anyone have some advice?&lt;/P&gt;&lt;P&gt;Best&lt;/P&gt;&lt;P&gt;Alessio&lt;/P&gt;</description>
      <pubDate>Fri, 05 Nov 2021 16:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367443#M3418</guid>
      <dc:creator>agalliazzo</dc:creator>
      <dc:date>2021-11-05T16:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z With SDK2.2.3 HardFault</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367661#M3419</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do you just use the example without any modification ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 05:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367661#M3419</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-11-08T05:35:59Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z With SDK2.2.3 HardFault</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367726#M3420</link>
      <description>&lt;P&gt;Hi, yes, it's a brand new demo project. No edit in the files. The network leader is an OpenThread based border router with a nrf52840 RCP.&lt;/P&gt;&lt;P&gt;With other development board from Nordic the network works without issues.&lt;/P&gt;&lt;P&gt;Best&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 07:22:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367726#M3420</guid>
      <dc:creator>agalliazzo</dc:creator>
      <dc:date>2021-11-08T07:22:16Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z With SDK2.2.3 HardFault</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367763#M3421</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I test on two frdm-kw41. It woks well. So may be the kw41 has&amp;nbsp;compatibility with other company's product. I do not have the Nordic product. I also can't test this problem.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Nov 2021 08:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/KW41Z-With-SDK2-2-3-HardFault/m-p/1367763#M3421</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-11-08T08:16:33Z</dc:date>
    </item>
  </channel>
</rss>