<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDK中的主题 Re: RT1050EVKB QSPI</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1290837#M3206</link>
    <description>&lt;P&gt;In the application note it states the chip does not have to be removed if the board is an EVKB. Is this true?&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jun 2021 15:52:47 GMT</pubDate>
    <dc:creator>scottdewey</dc:creator>
    <dc:date>2021-06-10T15:52:47Z</dc:date>
    <item>
      <title>RT1050EVKB QSPI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1288526#M3197</link>
      <description>&lt;P&gt;I am trying to get the QSPI to operate on the rt1050-EVKB.&lt;/P&gt;&lt;P&gt;I have so far:&lt;/P&gt;&lt;P&gt;So far I have:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;removed the resistors from the hyperflash&lt;/LI&gt;&lt;LI&gt;installed the needed 0 ohm resistors around the QSPI.&lt;/LI&gt;&lt;LI&gt;Updated the OpenSDA firmware to k20dx_mimxrt1050_evk_qspi_if_crc.bin&lt;/LI&gt;&lt;LI&gt;I have changed MIMXRT1050-EVK_S26KS512S.cfx&amp;nbsp;to MIMXRT1050-EVK_IS25WP064A.cfx&lt;/LI&gt;&lt;LI&gt;I have the QSPI Boot mode on the board set to: SW7-1 = 0 SW7-2=0 SW7-3=1 SW7-4=0&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;It looks like I am getting a few different errors starting with the connect script but it does look like the flash was successfully written.&amp;nbsp;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Jan 11 2021 16:41:13 - crt_emu_cm_redlink build 9)&lt;BR /&gt;Found chip XML file in C:/Users/DeweyS/Documents/MCUXpressoIDE_11.3.0_5222/workspace/evkbimxrt1050_hello_world/Debug\MIMXRT1052xxxxB.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1050_connect.scp =============&lt;BR /&gt;RT1050 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Error: Wire Ack Wait Fault&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: DAPLink CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 0227000047784e4500289004d745003addb1000097969900&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#7&amp;amp;cc7afd2&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;connection failed - Em(01). Cannot find MEM-AP selected by core index (check target power).. Retrying&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;On debug connection - reset using system reset&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1052xxxxB&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;BR /&gt;note - part information contained no product license-type data&lt;BR /&gt;Inspected v.2 External Flash Device on SPI MIMXRT1050-EVK_IS25WP064A.cfx&lt;BR /&gt;Image 'MIMXRT1050-EVK_IS25WP064A Dec 17 2020 10:04:52'&lt;BR /&gt;Connected: was_reset=false. was_stopped=true&lt;BR /&gt;Awaiting telnet connection to port 3332 ...&lt;BR /&gt;GDB nonstop mode enabled&lt;BR /&gt;Opening flash driver MIMXRT1050-EVK_IS25WP064A.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Flash device supported (8MB = 128*64K at 0x60000000)&lt;BR /&gt;Writing 24124 bytes to address 0x60000000 in Flash&lt;BR /&gt;Sectors written: 0, unchanged: 1, total: 1&lt;BR /&gt;Erased/Wrote sector 0-0 with 24124 bytes in 15msec&lt;BR /&gt;Closing flash driver MIMXRT1050-EVK_IS25WP064A.cfx&lt;BR /&gt;Flash Write Done&lt;BR /&gt;Flash Program Summary: 24124 bytes in 0.01 seconds (1570.57 KB/sec)&lt;BR /&gt;============= SCRIPT: CTNxxx_Connect.scp =============&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;following reset read of core registers failed - Ep(08). Cannot access core regs when target running.&lt;BR /&gt;Target error from Commit Flash write: Ep(08). Cannot access core regs when target running.&lt;BR /&gt;GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;BR /&gt;state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;/P&gt;&lt;P&gt;I hope someone can help me get through this.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jun 2021 19:29:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1288526#M3197</guid>
      <dc:creator>scottdewey</dc:creator>
      <dc:date>2021-06-07T19:29:04Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050EVKB QSPI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1289987#M3200</link>
      <description>&lt;P&gt;Hi Scott,&lt;/P&gt;
&lt;P&gt;Did you remove the onboard Hyper Flash? If not, this will impact the QSPI Flash read and write timing. Please check the application note below that explains this process in detail.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12108.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12108.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Felipe&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note:&lt;/P&gt;
&lt;P&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 15:36:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1289987#M3200</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2021-06-09T15:36:42Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050EVKB QSPI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1290837#M3206</link>
      <description>&lt;P&gt;In the application note it states the chip does not have to be removed if the board is an EVKB. Is this true?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jun 2021 15:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1290837#M3206</guid>
      <dc:creator>scottdewey</dc:creator>
      <dc:date>2021-06-10T15:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: RT1050EVKB QSPI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1292534#M3210</link>
      <description>&lt;P&gt;The NXP support response of using AN12108 was of no help. I did receive some guidance from a different NXP source. The fix is below:&lt;/P&gt;&lt;P&gt;so apparently the guide does not mention that there needs to be a software modification. You need to go into the &lt;STRONG&gt;evkbimxrt1050_flexspi_nor_config.c&lt;/STRONG&gt;, contained in the XIP directory; then you need to modify the configuration struct:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;const flexspi_nor_config_t hyperflash_config = {...}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;Add this code:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;const flexspi_nor_config_t qspiflash_config = {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; .memConfig =&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .tag &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= FLEXSPI_CFG_BLK_TAG,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .version &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= FLEXSPI_CFG_BLK_VERSION,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackFromDqsPad,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .csHoldTime &amp;nbsp; &amp;nbsp; &amp;nbsp; = 3u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .csSetupTime &amp;nbsp; &amp;nbsp; &amp;nbsp;= 3u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .sflashPadType &amp;nbsp; &amp;nbsp;= kSerialFlash_4Pads,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .serialClkFreq &amp;nbsp; &amp;nbsp;= kFlexSpiSerialClk_100MHz,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .sflashA1Size &amp;nbsp; &amp;nbsp; = 8u * 1024u * 1024u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; .lookupTable =&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; // Read LUTs&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; },&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; },&lt;BR /&gt;&amp;nbsp; &amp;nbsp; .pageSize &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 256u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; .sectorSize &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; = 4u * 1024u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; .blockSize &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;= 64u * 1024u,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; .isUniformBlockSize = false,&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;I have attached the working code.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jun 2021 10:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/RT1050EVKB-QSPI/m-p/1292534#M3210</guid>
      <dc:creator>scottdewey</dc:creator>
      <dc:date>2021-06-15T10:44:13Z</dc:date>
    </item>
  </channel>
</rss>