<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: LPI2C_MasterTransferNonBlocking() Not Starting</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPI2C-MasterTransferNonBlocking-Not-Starting/m-p/1286505#M3193</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;chadgraham,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I can't find any problem in this short piece of code. Since none blocking function need interrupt, please check other related part and LPI2C initialize code. If the&amp;nbsp;lpi2c_interrupt_b2b_transfer_master&amp;nbsp;example can run well on your board, there should not be hardware problem.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Jun 2021 03:01:06 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-06-03T03:01:06Z</dc:date>
    <item>
      <title>LPI2C_MasterTransferNonBlocking() Not Starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPI2C-MasterTransferNonBlocking-Not-Starting/m-p/1285602#M3190</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to convert from a basic I2C implementation to one that uses the non-blocking functions.&amp;nbsp; Using the lpi2c_interrupt_b2b_transfer_master example, I converted my read function to use&amp;nbsp;LPI2C_MasterTransferNonBlocking(), but I am unable to get the I2C function to do anything on the bus even though it returns&amp;nbsp;kStatus_Success and the handle now contains the data.&amp;nbsp; Converting it to&amp;nbsp;LPI2C_MasterTransferBlocking causes the data to be sent so I'm certain that the setup portion is still working.&lt;/P&gt;&lt;P&gt;That said, I am suspecting that the handle may be the culprit.&amp;nbsp; If I hover over the handle after issuing the&amp;nbsp;LPI2C_MasterTransferNonBlocking command, I can see that the handle has the correct information, but it seems to just stay in the '1' state.&lt;/P&gt;&lt;P&gt;Has anyone else experienced this kind of thing?&amp;nbsp; I've attached a slightly modified example of my read stream function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jun 2021 19:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/LPI2C-MasterTransferNonBlocking-Not-Starting/m-p/1285602#M3190</guid>
      <dc:creator>chadgraham</dc:creator>
      <dc:date>2021-06-01T19:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPI2C_MasterTransferNonBlocking() Not Starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/LPI2C-MasterTransferNonBlocking-Not-Starting/m-p/1286505#M3193</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;chadgraham,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I can't find any problem in this short piece of code. Since none blocking function need interrupt, please check other related part and LPI2C initialize code. If the&amp;nbsp;lpi2c_interrupt_b2b_transfer_master&amp;nbsp;example can run well on your board, there should not be hardware problem.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jing&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jun 2021 03:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/LPI2C-MasterTransferNonBlocking-Not-Starting/m-p/1286505#M3193</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-06-03T03:01:06Z</dc:date>
    </item>
  </channel>
</rss>