<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ThreadX + NetX example for iMXRT1010 in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/ThreadX-NetX-example-for-iMXRT1010/m-p/1276140#M3167</link>
    <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;We are working on a project&amp;nbsp; which uses ThreadX + NetX Code in the application. we have LTE module in our product. So, we do not need ethernet in our application . However we need network stack.&lt;/P&gt;&lt;P&gt;We need to port the application to iMXRT1010 MCU.&lt;/P&gt;&lt;P&gt;We tried to find NetX demo in the MCU Xpresso SDK. But, we&amp;nbsp; are not able to find any example for the same. We are using SDK generated from &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1010" target="_self"&gt;Here&amp;nbsp;&amp;nbsp;&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Can you help us to find the example code for the same.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hiren Bhuba&lt;/P&gt;</description>
    <pubDate>Thu, 13 May 2021 03:58:44 GMT</pubDate>
    <dc:creator>Hiren_Bhuva</dc:creator>
    <dc:date>2021-05-13T03:58:44Z</dc:date>
    <item>
      <title>ThreadX + NetX example for iMXRT1010</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/ThreadX-NetX-example-for-iMXRT1010/m-p/1276140#M3167</link>
      <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;We are working on a project&amp;nbsp; which uses ThreadX + NetX Code in the application. we have LTE module in our product. So, we do not need ethernet in our application . However we need network stack.&lt;/P&gt;&lt;P&gt;We need to port the application to iMXRT1010 MCU.&lt;/P&gt;&lt;P&gt;We tried to find NetX demo in the MCU Xpresso SDK. But, we&amp;nbsp; are not able to find any example for the same. We are using SDK generated from &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1010" target="_self"&gt;Here&amp;nbsp;&amp;nbsp;&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Can you help us to find the example code for the same.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hiren Bhuba&lt;/P&gt;</description>
      <pubDate>Thu, 13 May 2021 03:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/ThreadX-NetX-example-for-iMXRT1010/m-p/1276140#M3167</guid>
      <dc:creator>Hiren_Bhuva</dc:creator>
      <dc:date>2021-05-13T03:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: ThreadX + NetX example for iMXRT1010</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/ThreadX-NetX-example-for-iMXRT1010/m-p/1276863#M3169</link>
      <description>&lt;P&gt;Hi Hiren_Bhuva,&lt;/P&gt;
&lt;P&gt;RT1010 hasn't ENET interface, so its SDK hasn't ethernet example. You can download RT1060 SDK. It has threadx example and netX example in azure_rtos_examples folder. But you have to port these examples to RT1010.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Fri, 14 May 2021 08:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/ThreadX-NetX-example-for-iMXRT1010/m-p/1276863#M3169</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-05-14T08:03:38Z</dc:date>
    </item>
  </channel>
</rss>