<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: Can one reinitialize a function of USB composite device?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Can-one-reinitialize-a-function-of-USB-composite-device/m-p/1260819#M3123</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Marek,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;With reinitialization, you mean to restart the process of enumeration and identification? If so, is not possible to reinitialize the&amp;nbsp;USB-MTP without breaking the communication with the&amp;nbsp;USB-CDC.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 13 Apr 2021 00:40:52 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2021-04-13T00:40:52Z</dc:date>
    <item>
      <title>Can one reinitialize a function of USB composite device?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Can-one-reinitialize-a-function-of-USB-composite-device/m-p/1259611#M3122</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm working on a UBS composite device, which consists of USB-CDC and USB-MTP functions. In one of the use cases, I'd like to be able to reinitialize MTP functionality without breaking USB-CDC communication. Using the following sequence works for MTP, but breaks CDC.&lt;/P&gt;&lt;P&gt;```&lt;BR /&gt;USB_DeviceStop();&lt;BR /&gt;&lt;SPAN&gt;USB_DeviceSetIsr(false);&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;MtpReinit();&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;USB_DeviceSetIsr(true);&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;USB_DeviceRun();&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;```&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Marek&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 09 Apr 2021 10:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Can-one-reinitialize-a-function-of-USB-composite-device/m-p/1259611#M3122</guid>
      <dc:creator>niepiekm</dc:creator>
      <dc:date>2021-04-09T10:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: Can one reinitialize a function of USB composite device?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Can-one-reinitialize-a-function-of-USB-composite-device/m-p/1260819#M3123</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Marek,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;With reinitialization, you mean to restart the process of enumeration and identification? If so, is not possible to reinitialize the&amp;nbsp;USB-MTP without breaking the communication with the&amp;nbsp;USB-CDC.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards,&lt;BR /&gt;Victor&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 00:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Can-one-reinitialize-a-function-of-USB-composite-device/m-p/1260819#M3123</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2021-04-13T00:40:52Z</dc:date>
    </item>
  </channel>
</rss>