<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックSDK Details: Devices &amp;quot;not installed&amp;quot;</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/1230543#M3062</link>
    <description>&lt;P&gt;I'm migrating from LPC1769 to LPC55S28 so I had the pleasure to use the SDK facility for the first time.&lt;/P&gt;&lt;P&gt;You are reporting a "not installed" message in SDK Details. I also saw this message in SDK Details, see screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1613155547903.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137130i99BDC179C29941B2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielholala_0-1613155547903.png" alt="danielholala_0-1613155547903.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In my case, the "not installed" message was caused by having two SDKs installed with both SDKs containing the same part support.&lt;/P&gt;&lt;P&gt;The excellent documentation explains this message, see&amp;nbsp;"MCUXpresso IDE User Guide Rev. 11.3.0", page 37, Section&amp;nbsp;4.2.8 "Important notes for SDK Users":&lt;/P&gt;&lt;P&gt;"...If both SDKs are installed into the IDE, both sets of examples and&lt;BR /&gt;board drivers will be available, but the IDE will select the most up to date version of part support&lt;BR /&gt;specified within these SDKs."&lt;/P&gt;&lt;P&gt;I "uninstalled" the other SDK and now the part support is taken from this SDK.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Feb 2021 18:54:49 GMT</pubDate>
    <dc:creator>danielholala</dc:creator>
    <dc:date>2021-02-12T18:54:49Z</dc:date>
    <item>
      <title>Device Not Installed in SDK 2.4</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/754434#M591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've just migrated to the newest MCUXpresso IDE 10.2 and did a drag drop install of the 2.4 SDK.&amp;nbsp; When I look at the SDK details I see the note under Devices MK66F18 (not installed) 1.0.0.&amp;nbsp; This is also the case for MK65F18.&amp;nbsp; I'd just ignore it, but I'm running into a hard fault that I cannot seem to resolve.&amp;nbsp; Perhaps another question is in order for that.&amp;nbsp; Any knowledge on this out there?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jun 2018 18:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/754434#M591</guid>
      <dc:creator>jeremyanderson</dc:creator>
      <dc:date>2018-06-05T18:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: Device Not Installed in SDK 2.4</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/754435#M592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;Could you please take a screenshot about the information you mentioned.&lt;/P&gt;&lt;P&gt;Also please tell me which chip or board of your SDK package , and also tell me your test board,&lt;/P&gt;&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 10:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/754435#M592</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-06-06T10:24:49Z</dc:date>
    </item>
    <item>
      <title>SDK Details: Devices "not installed"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/1230543#M3062</link>
      <description>&lt;P&gt;I'm migrating from LPC1769 to LPC55S28 so I had the pleasure to use the SDK facility for the first time.&lt;/P&gt;&lt;P&gt;You are reporting a "not installed" message in SDK Details. I also saw this message in SDK Details, see screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielholala_0-1613155547903.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137130i99BDC179C29941B2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielholala_0-1613155547903.png" alt="danielholala_0-1613155547903.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In my case, the "not installed" message was caused by having two SDKs installed with both SDKs containing the same part support.&lt;/P&gt;&lt;P&gt;The excellent documentation explains this message, see&amp;nbsp;"MCUXpresso IDE User Guide Rev. 11.3.0", page 37, Section&amp;nbsp;4.2.8 "Important notes for SDK Users":&lt;/P&gt;&lt;P&gt;"...If both SDKs are installed into the IDE, both sets of examples and&lt;BR /&gt;board drivers will be available, but the IDE will select the most up to date version of part support&lt;BR /&gt;specified within these SDKs."&lt;/P&gt;&lt;P&gt;I "uninstalled" the other SDK and now the part support is taken from this SDK.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Feb 2021 18:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Device-Not-Installed-in-SDK-2-4/m-p/1230543#M3062</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2021-02-12T18:54:49Z</dc:date>
    </item>
  </channel>
</rss>