<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UID for Kinetis with SDK in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/UID-for-Kinetis-with-SDK/m-p/1191288#M2912</link>
    <description>&lt;P&gt;As a heads-up: The MCUXpresso SDK&amp;nbsp;&lt;SPAN&gt;SIM_GetUniqueId() function can be used to retrieve the unique ID (UID) of the part. I noticed that with using the SDK only 96 of the available 128 bits are retrieved.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm using the SDK 2.8.2, and as a workaround I had to set the SIM_UIDH defined.&lt;/P&gt;&lt;P&gt;More details in&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2020/11/30/getting-a-96bit-unique-id-for-each-kinetis-device-using-mcuxpresso-sdk/" target="_blank"&gt;Getting a 96bit Unique ID for each Kinetis Device using MCUXpresso SDK | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So if you need the full bits, make sure you set that define. I hope this will be fixed in an updated version oft the SDK.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 01 Dec 2020 05:29:43 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2020-12-01T05:29:43Z</dc:date>
    <item>
      <title>UID for Kinetis with SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/UID-for-Kinetis-with-SDK/m-p/1191288#M2912</link>
      <description>&lt;P&gt;As a heads-up: The MCUXpresso SDK&amp;nbsp;&lt;SPAN&gt;SIM_GetUniqueId() function can be used to retrieve the unique ID (UID) of the part. I noticed that with using the SDK only 96 of the available 128 bits are retrieved.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm using the SDK 2.8.2, and as a workaround I had to set the SIM_UIDH defined.&lt;/P&gt;&lt;P&gt;More details in&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2020/11/30/getting-a-96bit-unique-id-for-each-kinetis-device-using-mcuxpresso-sdk/" target="_blank"&gt;Getting a 96bit Unique ID for each Kinetis Device using MCUXpresso SDK | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So if you need the full bits, make sure you set that define. I hope this will be fixed in an updated version oft the SDK.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 05:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/UID-for-Kinetis-with-SDK/m-p/1191288#M2912</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2020-12-01T05:29:43Z</dc:date>
    </item>
  </channel>
</rss>