<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: FRDM-K66 FreeRTOS DSPI Pin-Muxing</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701589#M283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PTB23 is on pin9 of J4, not J3. Please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29061i20324FC62340F9FB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Aug 2017 08:42:03 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2017-08-22T08:42:03Z</dc:date>
    <item>
      <title>FRDM-K66 FreeRTOS DSPI Pin-Muxing</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701588#M282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've created a project for this example and run it with success, but just for educational purposes I changed the pin muxing to use SPI2 so the jumpering looks like this:&lt;/P&gt;&lt;P&gt;SPI0 pins are connected with SPI1 pins of board&lt;BR /&gt;INSTANCE0&amp;nbsp;&amp;nbsp;&amp;nbsp;(SPI0) CONNECTS TO &amp;nbsp;&amp;nbsp;&amp;nbsp;INSTANCE1(SPI2)&lt;BR /&gt;Pin Name&amp;nbsp;&amp;nbsp;&amp;nbsp; Board Location&amp;nbsp;&amp;nbsp;&amp;nbsp; Pin Name Board Location&lt;BR /&gt;MOSI &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 10 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MISO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 17&lt;BR /&gt;MISO &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 8 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;MOSI &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J3 pin 9&lt;BR /&gt;SCK &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 12 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;SCK &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 19&lt;BR /&gt;PCS0 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J2 pin 6 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;PCS0 &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;J6 pin 3&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After using the Pin Tool to generate the pinmux files I copied them in to my project and changed:&lt;/P&gt;&lt;P&gt;#define EXAMPLE_DSPI_SLAVE_BASE (SPI1_BASE)&lt;BR /&gt;#define EXAMPLE_DSPI_SLAVE_IRQN (SPI1_IRQn)&lt;/P&gt;&lt;P&gt;to:&lt;/P&gt;&lt;P&gt;#define EXAMPLE_DSPI_SLAVE_BASE (SPI2_BASE)&lt;BR /&gt;#define EXAMPLE_DSPI_SLAVE_IRQN (SPI2_IRQn)&lt;/P&gt;&lt;P&gt;When I run this example I get an error reported in data transfer. &amp;nbsp;The master and slave transfers complete successfully, but the data received by the slave is all 1s, whereas the data received by the master matches what was sent by the slave.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm wondering is this is a problem with the documentation of the board or the pin muxing, or if I don't understand the process. &amp;nbsp;Anyone else tried this?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338860"&gt;pin_mux.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338860"&gt;pin_mux.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Aug 2017 14:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701588#M282</guid>
      <dc:creator>jeremyanderson</dc:creator>
      <dc:date>2017-08-18T14:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66 FreeRTOS DSPI Pin-Muxing</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701589#M283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PTB23 is on pin9 of J4, not J3. Please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29061i20324FC62340F9FB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 08:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701589#M283</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2017-08-22T08:42:03Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K66 FreeRTOS DSPI Pin-Muxing</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701590#M284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that solved my problem and the lesson for me was to not trust the labels in the imported project. &amp;nbsp;;-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 14:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-K66-FreeRTOS-DSPI-Pin-Muxing/m-p/701590#M284</guid>
      <dc:creator>jeremyanderson</dc:creator>
      <dc:date>2017-08-22T14:29:15Z</dc:date>
    </item>
  </channel>
</rss>