<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failed when assert(serialHandle); in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085404#M2647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have a solution yet. I am not using that feature. Just that when I generate the example, I saw this issue. I had proceeded with other tests.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2020 23:53:25 GMT</pubDate>
    <dc:creator>alan5</dc:creator>
    <dc:date>2020-05-06T23:53:25Z</dc:date>
    <item>
      <title>Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085401#M2644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I am working on LPCXpresso54608. I am running on an example to control LED in the shell. But there is an error when&amp;nbsp;assert(serialHandle); with the error message captured&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class=""&gt;ASSERT ERROR " .fsl_shell.c:820 : serialHandle&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;The code that I am using is generated by MCUXpresso.&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;/P&gt;&lt;P class=""&gt;Thank You!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2020 01:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085401#M2644</guid>
      <dc:creator>alan5</dc:creator>
      <dc:date>2020-04-13T01:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085402#M2645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please share the detailed process you are following so I can replicate this issue on my side?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 18:14:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085402#M2645</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-04-15T18:14:33Z</dc:date>
    </item>
    <item>
      <title>Re: Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085403#M2646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also getting same problem running &lt;STRONG&gt;frdmkl27z_shell&lt;/STRONG&gt; example project straight out the box from the frdm_kl27z demo examples.&lt;/P&gt;&lt;P&gt;The example is being run in the default DEBUG configuration.&lt;/P&gt;&lt;P&gt;The other semihosting example called frdmkl27z_hello_world works perfectly.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99768i0C197627A07C08FC/image-size/large?v=v2&amp;amp;px=999" title="assertfail1.png" alt="assertfail1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The Assert fails because SerialHandle is null.&lt;/P&gt;&lt;P&gt;If Alan found a fix I would be interested to know what it is.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2020 21:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085403#M2646</guid>
      <dc:creator>admin6</dc:creator>
      <dc:date>2020-04-30T21:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085404#M2647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have a solution yet. I am not using that feature. Just that when I generate the example, I saw this issue. I had proceeded with other tests.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2020 23:53:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085404#M2647</guid>
      <dc:creator>alan5</dc:creator>
      <dc:date>2020-05-06T23:53:25Z</dc:date>
    </item>
    <item>
      <title>Re: Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085405#M2648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I checked the example on my side using my LPCXpresso54608 board and it worked as expected. Please check the below image.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/106381i93B255AD90D33F65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I used MCUXpresso 11.1.1 and SDK 2.7.0 to test it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 14:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085405#M2648</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2020-05-13T14:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: Failed when assert(serialHandle);</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085406#M2649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan,&lt;/P&gt;&lt;P&gt;&amp;nbsp; The solution is to ensure that;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SDK Import Wizard&amp;nbsp; -&amp;gt;&amp;nbsp;&amp;nbsp; SDK Debug Console&amp;nbsp;&amp;nbsp; = UART&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (not Semihost! The default)&lt;/P&gt;&lt;P&gt;&amp;nbsp;as shown below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(Also you need to give the second attempt at importing this project a suffix so that the [Next] and [Finish] buttons are ungreyed - allowing you to proceed.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The imported project settings do NOT control the "SDK Debug Console" setting. You have to set it manually.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107297i59EFCF819F31F00C/image-size/large?v=v2&amp;amp;px=999" title="shellwiz2.png" alt="shellwiz2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards, and Thank you Felipe,&lt;/P&gt;&lt;P&gt;Rob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2020 19:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Failed-when-assert-serialHandle/m-p/1085406#M2649</guid>
      <dc:creator>admin6</dc:creator>
      <dc:date>2020-05-14T19:55:34Z</dc:date>
    </item>
  </channel>
</rss>