<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックRe: FRDM-KL46Z FreeRTOS example UART and SPI Project Issues</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-KL46Z-FreeRTOS-example-UART-and-SPI-Project-Issues/m-p/1071555#M2492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Konstantinos:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer to the readme&amp;nbsp; txt file under the demo folder.&lt;/P&gt;&lt;P&gt;for instance, For freertos uart project,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware requirements&lt;BR /&gt;=====================&lt;BR /&gt;- Mini USB cable&lt;BR /&gt;- FRDM-KL46Z board&lt;BR /&gt;- Personal Computer&lt;BR /&gt;- USB to Com Converter&lt;/P&gt;&lt;P&gt;Board settings&lt;BR /&gt;==============&lt;BR /&gt;USB2COM UART1&lt;BR /&gt;Pin Name Pin Name Board Location&lt;BR /&gt;RX PTE0 J2 pin 18&lt;BR /&gt;TX PTE1 J2 pin 20&lt;BR /&gt;GND GND J2 pin 14&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please check your board settings ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2020 06:43:50 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2020-07-23T06:43:50Z</dc:date>
    <item>
      <title>FRDM-KL46Z FreeRTOS example UART and SPI Project Issues</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-KL46Z-FreeRTOS-example-UART-and-SPI-Project-Issues/m-p/1071554#M2491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, this is my first time using an ARM board, so I know so little. I have a FreeRTOS university project that utilises UART and SPI, so I was instructed to load the example SDK projects to familiarise myself. However, I've stumbled into some issues trying to run them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the freertos_uart project, I use Tera Term as my terminal and I adjust the serial port settings as the project suggests. I believe I've done so correctly:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116505iF94692161A10EE4A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From what I can see, the project should sent some text to the terminal, but it doesn't seem to work in my case; the window remains blank. Do I need to adjust some extra project/Tera Term properties for it to work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for freertos_spi project, I run the project, which sends some data and then receives it. I get multiple mismatch errors when data is received:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/116506i18A63F75E79405BE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How could I get these projects to work? Maybe I should also note that I run MCUXpresso in a virtual machine with Windows 7 because running directly on Windows 10 had caused my board's bootloader to become corrupted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2020 17:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-KL46Z-FreeRTOS-example-UART-and-SPI-Project-Issues/m-p/1071554#M2491</guid>
      <dc:creator>p17085</dc:creator>
      <dc:date>2020-07-21T17:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KL46Z FreeRTOS example UART and SPI Project Issues</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-KL46Z-FreeRTOS-example-UART-and-SPI-Project-Issues/m-p/1071555#M2492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Konstantinos:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer to the readme&amp;nbsp; txt file under the demo folder.&lt;/P&gt;&lt;P&gt;for instance, For freertos uart project,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware requirements&lt;BR /&gt;=====================&lt;BR /&gt;- Mini USB cable&lt;BR /&gt;- FRDM-KL46Z board&lt;BR /&gt;- Personal Computer&lt;BR /&gt;- USB to Com Converter&lt;/P&gt;&lt;P&gt;Board settings&lt;BR /&gt;==============&lt;BR /&gt;USB2COM UART1&lt;BR /&gt;Pin Name Pin Name Board Location&lt;BR /&gt;RX PTE0 J2 pin 18&lt;BR /&gt;TX PTE1 J2 pin 20&lt;BR /&gt;GND GND J2 pin 14&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;could you please check your board settings ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2020 06:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/FRDM-KL46Z-FreeRTOS-example-UART-and-SPI-Project-Issues/m-p/1071555#M2492</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2020-07-23T06:43:50Z</dc:date>
    </item>
  </channel>
</rss>