<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SRAM_LOWER utilization in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/SRAM-LOWER-utilization/m-p/690342#M239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the assumption that you are using MCUXpresso IDE, then please see chapter 12, "Memory Configuration and Linker Scripts", of the MCUXpresso IDE v10.0. User Guide for more details of how images are laid out in memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are various ways of moving the&amp;nbsp;heap, stack or&amp;nbsp;global variables into the second RAM bank described in this chapter - the simplest of which is probably to use the "Heap and Stack placement" editor, as shown in section 12.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Jun 2017 15:25:39 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-06-19T15:25:39Z</dc:date>
    <item>
      <title>SRAM_LOWER utilization</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/SRAM-LOWER-utilization/m-p/690341#M238</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso SDK build for Kinetis MK02FN64xxxx10 which has 8 kB + 8 kB SRAM memory.&amp;nbsp;All the variables are stored only in upper memory. When I reach 8 kB, the&amp;nbsp;Console return me&amp;nbsp;region `SRAM_UPPER' overflowed and the&amp;nbsp;SRAM_LOWER still remain empty. How to use the SRAM_LOWER ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Jun 2017 08:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/SRAM-LOWER-utilization/m-p/690341#M238</guid>
      <dc:creator>Jan321</dc:creator>
      <dc:date>2017-06-18T08:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM_LOWER utilization</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/SRAM-LOWER-utilization/m-p/690342#M239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the assumption that you are using MCUXpresso IDE, then please see chapter 12, "Memory Configuration and Linker Scripts", of the MCUXpresso IDE v10.0. User Guide for more details of how images are laid out in memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are various ways of moving the&amp;nbsp;heap, stack or&amp;nbsp;global variables into the second RAM bank described in this chapter - the simplest of which is probably to use the "Heap and Stack placement" editor, as shown in section 12.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 15:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/SRAM-LOWER-utilization/m-p/690342#M239</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-06-19T15:25:39Z</dc:date>
    </item>
  </channel>
</rss>