<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso SDKのトピックSAI/I2S Example for FRDM-K64f</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/SAI-I2S-Example-for-FRDM-K64f/m-p/1044771#M2308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm using the FRDM-K64F Board and try to connect it via I2S to an external I2S Microphone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Are there any SAI Examples for this board?&lt;/LI&gt;&lt;LI&gt;Or maybe Example for similar Board, such i could addept it for the FRDM-K64f?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;I know from the SDK documentation that there should be examples for other boards. Any suggestions which Example from which other Board i could use?&lt;BR /&gt;&lt;BR /&gt;Best&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jul 2020 16:25:06 GMT</pubDate>
    <dc:creator>nteschner</dc:creator>
    <dc:date>2020-07-30T16:25:06Z</dc:date>
    <item>
      <title>SAI/I2S Example for FRDM-K64f</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/SAI-I2S-Example-for-FRDM-K64f/m-p/1044771#M2308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i'm using the FRDM-K64F Board and try to connect it via I2S to an external I2S Microphone:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Are there any SAI Examples for this board?&lt;/LI&gt;&lt;LI&gt;Or maybe Example for similar Board, such i could addept it for the FRDM-K64f?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;I know from the SDK documentation that there should be examples for other boards. Any suggestions which Example from which other Board i could use?&lt;BR /&gt;&lt;BR /&gt;Best&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 16:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/SAI-I2S-Example-for-FRDM-K64f/m-p/1044771#M2308</guid>
      <dc:creator>nteschner</dc:creator>
      <dc:date>2020-07-30T16:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: SAI/I2S Example for FRDM-K64f</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/SAI-I2S-Example-for-FRDM-K64f/m-p/1044772#M2309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-size: small;"&gt;The attachment is the twr-k60's i2s. You can refer it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 00:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/SAI-I2S-Example-for-FRDM-K64f/m-p/1044772#M2309</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2020-07-31T00:57:59Z</dc:date>
    </item>
  </channel>
</rss>