<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there any non-blocking function for QN9080? in MCUXpresso SDK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-SDK/Is-there-any-non-blocking-function-for-QN9080/m-p/1038620#M2227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using QN9080 DK connected to a computer via USB port(UART), and I have a while loop&amp;nbsp;which is necessary to work in this loop until user press any key on the keyboard. Is there any non-blocking function for this? (I need an unblocking function such as "kbhit") or something that can reset the microcontroller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2019 13:18:41 GMT</pubDate>
    <dc:creator>ashkanrezaee</dc:creator>
    <dc:date>2019-11-26T13:18:41Z</dc:date>
    <item>
      <title>Is there any non-blocking function for QN9080?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Is-there-any-non-blocking-function-for-QN9080/m-p/1038620#M2227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using QN9080 DK connected to a computer via USB port(UART), and I have a while loop&amp;nbsp;which is necessary to work in this loop until user press any key on the keyboard. Is there any non-blocking function for this? (I need an unblocking function such as "kbhit") or something that can reset the microcontroller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 13:18:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Is-there-any-non-blocking-function-for-QN9080/m-p/1038620#M2227</guid>
      <dc:creator>ashkanrezaee</dc:creator>
      <dc:date>2019-11-26T13:18:41Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any non-blocking function for QN9080?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-SDK/Is-there-any-non-blocking-function-for-QN9080/m-p/1038621#M2228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean by reset the MCU ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check the following examples ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;qn908xcdk_usb_examples_usb_device_cdc_vcom_freertos&lt;/P&gt;&lt;P&gt;qn908xcdk_usb_examples_usb_device_composite_hid_mouse_hid_keyboard_freertos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 15:57:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-SDK/Is-there-any-non-blocking-function-for-QN9080/m-p/1038621#M2228</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-11-26T15:57:49Z</dc:date>
    </item>
  </channel>
</rss>